<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックOptical microcontroller</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Optical-microcontroller/m-p/1841561#M195</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm looking for a microcontroller with on-chip IDACs, support for thermoelectric cooler control, on-chip temperature sensing circuits etc., for use as an optical signal processor and controller. Could you suggest some possible NXP microcontrollers/microprocessors?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sheema&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sat, 06 Apr 2024 07:33:50 GMT</pubDate>
    <dc:creator>SheemaEgbert</dc:creator>
    <dc:date>2024-04-06T07:33:50Z</dc:date>
    <item>
      <title>Optical microcontroller</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Optical-microcontroller/m-p/1841561#M195</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm looking for a microcontroller with on-chip IDACs, support for thermoelectric cooler control, on-chip temperature sensing circuits etc., for use as an optical signal processor and controller. Could you suggest some possible NXP microcontrollers/microprocessors?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sheema&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 06 Apr 2024 07:33:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Optical-microcontroller/m-p/1841561#M195</guid>
      <dc:creator>SheemaEgbert</dc:creator>
      <dc:date>2024-04-06T07:33:50Z</dc:date>
    </item>
    <item>
      <title>Re: Optical microcontroller</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Optical-microcontroller/m-p/1841612#M197</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that all the on-chip DACs for MCU are voltage output DAC instead of current output DAC.&lt;/P&gt;
&lt;P&gt;For you application of iDAC, you can use on-chip DAC of MCU to output voltage from DAC_OUTPUT pin, then connect the DAC_OUTPUT pin to an external OP AMP and a transistor/MOSFET to output current.&lt;/P&gt;
&lt;P&gt;The MCXN fanily has 14 bits resolution on-chip voltage output DAC.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/mcx-arm-cortex-m/mcx-n-series-microcontrollers:MCX-N-SERIES" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/mcx-arm-cortex-m/mcx-n-series-microcontrollers:MCX-N-SERIES&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The other family, for example LPC84x low cost MCU also has on-chip voltage output DAC.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Sun, 07 Apr 2024 01:57:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Optical-microcontroller/m-p/1841612#M197</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-04-07T01:57:08Z</dc:date>
    </item>
    <item>
      <title>Re: Optical microcontroller</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Optical-microcontroller/m-p/1841707#M199</link>
      <description>&lt;P&gt;Thanks, XianJun, this clears the part about the current DACs.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 07 Apr 2024 06:52:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Optical-microcontroller/m-p/1841707#M199</guid>
      <dc:creator>SheemaEgbert</dc:creator>
      <dc:date>2024-04-07T06:52:49Z</dc:date>
    </item>
  </channel>
</rss>