<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB composite device in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/USB-composite-device/m-p/1982500#M1836</link>
    <description>&lt;P&gt;HI NXP,&lt;/P&gt;&lt;P&gt;We are developing a USB compostie device based on the NXP SDK_2_14_0_FRDM-MCXN236_rfp USB device example, with an MCTP class (using endpoints 1 and 2) and an HID class (using endpoints 3 and 4).&lt;/P&gt;&lt;P&gt;I modified the following:&lt;/P&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;SPAN class=""&gt;#&lt;SPAN class=""&gt;define&lt;/SPAN&gt; USB_DEVICE_CONFIG_ENDPOINTS (5U)&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;I found that only endpoints 1 and 2 work—the MCTP class functions correctly, but the HID class does not.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However, when I change it to use the MCTP class on endpoints 3 and 4 and the HID class on endpoints 1 and 2, the HID class works, but the MCTP class does not.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you tell me if the endpoint settings need to be modified?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Alan&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 27 Oct 2024 17:37:16 GMT</pubDate>
    <dc:creator>allu</dc:creator>
    <dc:date>2024-10-27T17:37:16Z</dc:date>
    <item>
      <title>USB composite device</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/USB-composite-device/m-p/1982500#M1836</link>
      <description>&lt;P&gt;HI NXP,&lt;/P&gt;&lt;P&gt;We are developing a USB compostie device based on the NXP SDK_2_14_0_FRDM-MCXN236_rfp USB device example, with an MCTP class (using endpoints 1 and 2) and an HID class (using endpoints 3 and 4).&lt;/P&gt;&lt;P&gt;I modified the following:&lt;/P&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;SPAN class=""&gt;#&lt;SPAN class=""&gt;define&lt;/SPAN&gt; USB_DEVICE_CONFIG_ENDPOINTS (5U)&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;I found that only endpoints 1 and 2 work—the MCTP class functions correctly, but the HID class does not.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However, when I change it to use the MCTP class on endpoints 3 and 4 and the HID class on endpoints 1 and 2, the HID class works, but the MCTP class does not.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you tell me if the endpoint settings need to be modified?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Alan&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 27 Oct 2024 17:37:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/USB-composite-device/m-p/1982500#M1836</guid>
      <dc:creator>allu</dc:creator>
      <dc:date>2024-10-27T17:37:16Z</dc:date>
    </item>
    <item>
      <title>Re: USB composite device</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/USB-composite-device/m-p/1985352#M1874</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/233046"&gt;@allu&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;There is a composite demo available in the SDK that also uses 5 endpoints. You might find it helpful to refer to this demo for configuration guidance.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_0-1730359308900.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/307872i8584F9A6CC0B4E9C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_0-1730359308900.png" alt="Alice_Yang_0-1730359308900.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 31 Oct 2024 07:22:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/USB-composite-device/m-p/1985352#M1874</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-10-31T07:22:56Z</dc:date>
    </item>
  </channel>
</rss>