<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックOPAMP/PGA used in motor control</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/OPAMP-PGA-used-in-motor-control/m-p/1982496#M1833</link>
    <description>&lt;P&gt;Is there any example how to use the OPAMP/ (Programmable operation amplifier) within motor control aplication?&lt;/P&gt;</description>
    <pubDate>Sun, 27 Oct 2024 16:28:13 GMT</pubDate>
    <dc:creator>erikraynolds</dc:creator>
    <dc:date>2024-10-27T16:28:13Z</dc:date>
    <item>
      <title>OPAMP/PGA used in motor control</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/OPAMP-PGA-used-in-motor-control/m-p/1982496#M1833</link>
      <description>&lt;P&gt;Is there any example how to use the OPAMP/ (Programmable operation amplifier) within motor control aplication?&lt;/P&gt;</description>
      <pubDate>Sun, 27 Oct 2024 16:28:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/OPAMP-PGA-used-in-motor-control/m-p/1982496#M1833</guid>
      <dc:creator>erikraynolds</dc:creator>
      <dc:date>2024-10-27T16:28:13Z</dc:date>
    </item>
    <item>
      <title>Re: OPAMP/PGA used in motor control</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/OPAMP-PGA-used-in-motor-control/m-p/1983421#M1851</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As you know that 3 phase current is required to construct 3 phase coordinator for FOC control,&amp;nbsp; so at least, 3 OP AMPs are required.&lt;/P&gt;
&lt;P&gt;The MCXN has on-chip OP AMPs with internal resistor network, but the current power stage board has on-board OP AMPs, so there is not solution to use internal OP AMPs to amplify the 3 phase current which are sample by connecting shunt resistor on the bottom branches.&lt;/P&gt;
&lt;P&gt;But using internal OP AMPs for FOC control are under way for MCXA family including redesigning the power stage board and MCXN processor board.&lt;/P&gt;
&lt;P&gt;We have OP AMP firmware in SDK package.&lt;/P&gt;
&lt;P&gt;You can download SDK package from the website:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://mcuxpresso.nxp.com/en" target="_blank"&gt;https://mcuxpresso.nxp.com/en&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1730171023528.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/307369iC0AFBEDF14AC7C69/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1730171023528.png" alt="xiangjun_rong_0-1730171023528.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Tue, 29 Oct 2024 03:05:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/OPAMP-PGA-used-in-motor-control/m-p/1983421#M1851</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-10-29T03:05:59Z</dc:date>
    </item>
  </channel>
</rss>