<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックRe: CCM_CLKO1 Giving Clock Signal at Reset</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/CCM-CLKO1-Giving-Clock-Signal-at-Reset/m-p/1962864#M1699</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;This is an expected behavior since reset state will change IOMUX register to configure the pin as CCM_CLKOX function and is changed until device tree is loaded.&lt;/P&gt;
&lt;P&gt;As you mention, U-boot/kernel does not causes this.&lt;/P&gt;
&lt;P&gt;If you change the IOMUX option before e.g. in SLP, you could reduce the time with the clock output at reset.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
    <pubDate>Thu, 26 Sep 2024 17:40:32 GMT</pubDate>
    <dc:creator>JorgeCas</dc:creator>
    <dc:date>2024-09-26T17:40:32Z</dc:date>
    <item>
      <title>CCM_CLKO1 Giving Clock Signal at Reset</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/CCM-CLKO1-Giving-Clock-Signal-at-Reset/m-p/1961761#M1693</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are using &lt;STRONG&gt;CCM_CLKO1&lt;/STRONG&gt; as a GPIO in our application, but we’re seeing a clock signal output at reset, which is not ideal for our setup. This behavior is shown in the attached oscilloscope screenshots.&lt;/P&gt;&lt;P&gt;Details:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;Environment:&lt;/STRONG&gt; The measurement was taken in SD card boot mode with and without the SD card inserted.&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Observation:&lt;/STRONG&gt; &lt;STRONG&gt;CCM_CLKO1&lt;/STRONG&gt; (and &lt;STRONG&gt;CCM_CLKO2&lt;/STRONG&gt;) gives a clock output at reset, even though we intend to use &lt;STRONG&gt;CCM_CLKO1&lt;/STRONG&gt; as a GPIO.&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Potential Cause:&lt;/STRONG&gt; This seems to occur earlier in the boot process and cannot be caused by our software (U-Boot/Kernel). We suspect it might be related to the boot flow, possibly the ROM loader.&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Concern:&lt;/STRONG&gt; This clock signal is problematic for our application, and we would like to know if this behavior is normal or if there’s a way to disable the clock output at reset so we can use &lt;STRONG&gt;CCM_CLKO1&lt;/STRONG&gt; as a GPIO without interference.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Any insights or recommendations on how to resolve this would be greatly appreciated!&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Wed, 25 Sep 2024 12:11:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/CCM-CLKO1-Giving-Clock-Signal-at-Reset/m-p/1961761#M1693</guid>
      <dc:creator>hamzaatifi</dc:creator>
      <dc:date>2024-09-25T12:11:48Z</dc:date>
    </item>
    <item>
      <title>Re: CCM_CLKO1 Giving Clock Signal at Reset</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/CCM-CLKO1-Giving-Clock-Signal-at-Reset/m-p/1962864#M1699</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;This is an expected behavior since reset state will change IOMUX register to configure the pin as CCM_CLKOX function and is changed until device tree is loaded.&lt;/P&gt;
&lt;P&gt;As you mention, U-boot/kernel does not causes this.&lt;/P&gt;
&lt;P&gt;If you change the IOMUX option before e.g. in SLP, you could reduce the time with the clock output at reset.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Thu, 26 Sep 2024 17:40:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/CCM-CLKO1-Giving-Clock-Signal-at-Reset/m-p/1962864#M1699</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2024-09-26T17:40:32Z</dc:date>
    </item>
  </channel>
</rss>