<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX Microcontrollers中的主题 Implement the low power support in FreeRTOS</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Implement-the-low-power-support-in-FreeRTOS/m-p/1941722#M1563</link>
    <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have an existing FreeRTOS project designed for a power-saving application, and I am preparing to migrate it to a new IC, the MCXC141.&lt;/P&gt;&lt;P&gt;In the old project, setting configUSE_TICKLESS_IDLE to 1 allowed the system to enter low power mode when tasks were idle, and the low power support feature provided by the manufacturer.&lt;/P&gt;&lt;P&gt;Here is a couple of questions:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Can I simply set configUSE_TICKLESS_IDLE to 1 to enable low power support on the new IC or the only way is&amp;nbsp;implemented by myself?&lt;/LI&gt;&lt;LI&gt;Are there any other methods to achieve low power support?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your help!&lt;/P&gt;</description>
    <pubDate>Wed, 28 Aug 2024 03:27:07 GMT</pubDate>
    <dc:creator>kein_sunion</dc:creator>
    <dc:date>2024-08-28T03:27:07Z</dc:date>
    <item>
      <title>Implement the low power support in FreeRTOS</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Implement-the-low-power-support-in-FreeRTOS/m-p/1941722#M1563</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have an existing FreeRTOS project designed for a power-saving application, and I am preparing to migrate it to a new IC, the MCXC141.&lt;/P&gt;&lt;P&gt;In the old project, setting configUSE_TICKLESS_IDLE to 1 allowed the system to enter low power mode when tasks were idle, and the low power support feature provided by the manufacturer.&lt;/P&gt;&lt;P&gt;Here is a couple of questions:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Can I simply set configUSE_TICKLESS_IDLE to 1 to enable low power support on the new IC or the only way is&amp;nbsp;implemented by myself?&lt;/LI&gt;&lt;LI&gt;Are there any other methods to achieve low power support?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your help!&lt;/P&gt;</description>
      <pubDate>Wed, 28 Aug 2024 03:27:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Implement-the-low-power-support-in-FreeRTOS/m-p/1941722#M1563</guid>
      <dc:creator>kein_sunion</dc:creator>
      <dc:date>2024-08-28T03:27:07Z</dc:date>
    </item>
    <item>
      <title>Re: Implement the low power support in FreeRTOS</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Implement-the-low-power-support-in-FreeRTOS/m-p/1943108#M1580</link>
      <description>&lt;P&gt;hi,&lt;A id="link_6" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239697" target="_self" aria-label="View Profile of kein_sunion"&gt;&lt;SPAN class=""&gt;kein_sunion&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The MCX C144 microcontroller are ideal for embedded applications that require low power consumption, flexibility, and cost effectiveness. It has multiple low-power modes, which need to be selected and configured according to specific needs.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The questions you raise are suggested in the introduction linked below.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://docs.nxp.com/bundle/AN14332/page/topics/introduction.html" target="_blank"&gt;Note about the source code in the document (nxp.com)&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;This link explains The MCXC444 microcontroller family provides an explanation ultra-low-power feature for the power sensitive market. This MCU family implements several low-power modes to meet this&amp;nbsp; requirement. The application note provides detailed information about each power mode and includes case examples in the&amp;nbsp; SDK power mode switch example demo.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Hope it can help you.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Xu Zhang&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Aug 2024 06:37:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Implement-the-low-power-support-in-FreeRTOS/m-p/1943108#M1580</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2024-08-29T06:37:30Z</dc:date>
    </item>
  </channel>
</rss>