<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SDRAM connection in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/SDRAM-connection/m-p/1924213#M1435</link>
    <description>&lt;P&gt;Hello, I hope you are well.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;FlexIO can emulate different parallel interfaces however it will be difficult to integrate parallel SDRAM as FlexIO only has 32 pins.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;One alternative to this is using a serial RAM so you can emulate the interface on FlexIO:&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN14175.pdf" target="_blank"&gt;Using FlexIO to emulate Quad SPI master (nxp.com)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Fri, 02 Aug 2024 18:21:50 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2024-08-02T18:21:50Z</dc:date>
    <item>
      <title>SDRAM connection</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/SDRAM-connection/m-p/1923038#M1422</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to use an SDRAM (64Mb Synchronous Dynamic RAM) in my design based on MCXN23x. I couldn't find any information or a sample circuit diagram about it. I found out that only there is a way to connect it using FLEXIO; but I'm unsure.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anybody have any idea or similar experience?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 01 Aug 2024 13:36:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/SDRAM-connection/m-p/1923038#M1422</guid>
      <dc:creator>Hessam_Shafaghi</dc:creator>
      <dc:date>2024-08-01T13:36:28Z</dc:date>
    </item>
    <item>
      <title>Re: SDRAM connection</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/SDRAM-connection/m-p/1924213#M1435</link>
      <description>&lt;P&gt;Hello, I hope you are well.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;FlexIO can emulate different parallel interfaces however it will be difficult to integrate parallel SDRAM as FlexIO only has 32 pins.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;One alternative to this is using a serial RAM so you can emulate the interface on FlexIO:&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN14175.pdf" target="_blank"&gt;Using FlexIO to emulate Quad SPI master (nxp.com)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Fri, 02 Aug 2024 18:21:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/SDRAM-connection/m-p/1924213#M1435</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2024-08-02T18:21:50Z</dc:date>
    </item>
  </channel>
</rss>