<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックMCXN236: Using FLEXIO pins as I2C slave</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN236-Using-FLEXIO-pins-as-I2C-slave/m-p/1920789#M1406</link>
    <description>&lt;P&gt;I want to use the MCXN236 as a peripheral device and use the FLEXIO pins for I2C communication. There is an example project in SDK "flexio_i2c_interrupt_lpi2c_transfer" but it only has the driver to acts as a controller.&amp;nbsp;Is there any example code/drivers to use these pins for the peripheral?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 30 Jul 2024 17:48:39 GMT</pubDate>
    <dc:creator>burcu</dc:creator>
    <dc:date>2024-07-30T17:48:39Z</dc:date>
    <item>
      <title>MCXN236: Using FLEXIO pins as I2C slave</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN236-Using-FLEXIO-pins-as-I2C-slave/m-p/1920789#M1406</link>
      <description>&lt;P&gt;I want to use the MCXN236 as a peripheral device and use the FLEXIO pins for I2C communication. There is an example project in SDK "flexio_i2c_interrupt_lpi2c_transfer" but it only has the driver to acts as a controller.&amp;nbsp;Is there any example code/drivers to use these pins for the peripheral?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jul 2024 17:48:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN236-Using-FLEXIO-pins-as-I2C-slave/m-p/1920789#M1406</guid>
      <dc:creator>burcu</dc:creator>
      <dc:date>2024-07-30T17:48:39Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN236: Using FLEXIO pins as I2C slave</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN236-Using-FLEXIO-pins-as-I2C-slave/m-p/1926507#M1456</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/236727"&gt;@burcu&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;No, unfortunately we do not provide examples of the FlexIO acting as an I2C target.&amp;nbsp; There had been an effort in the past to do this but it was abandoned as&amp;nbsp;it couldn’t fully meet the spec and ended up needing more shifter/timer resources than the I2C controller mode. (eg: more than 2 shifters and 2 timers).&amp;nbsp; It is more efficient in terms of FlexIO resources to use LPI2C for target mode and FlexIO for controller mode.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Chris&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Aug 2024 15:53:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN236-Using-FLEXIO-pins-as-I2C-slave/m-p/1926507#M1456</guid>
      <dc:creator>chris_brown</dc:creator>
      <dc:date>2024-08-06T15:53:12Z</dc:date>
    </item>
  </channel>
</rss>