<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX Microcontrollers中的主题 MCUXpresso eDMA use with LPI2C</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCUXpresso-eDMA-use-with-LPI2C/m-p/1829598#M135</link>
    <description>&lt;P&gt;This is a general question.&lt;/P&gt;&lt;P&gt;I have looked at the NXP provided edma slave board to board example project provided for the imxrt1050-evkb.&lt;/P&gt;&lt;P&gt;This project does not use the MCUXpresso peripheral configuration tool.&lt;/P&gt;&lt;P&gt;I have attempted to set the edma up for use with the lpi2c and I can't seem to get the edma working.&lt;/P&gt;&lt;P&gt;Is there a reason NXP did not enable the peripheral configuration tools for this demo?&lt;/P&gt;&lt;P&gt;It's seems as though all set up is done manually.&lt;/P&gt;&lt;P&gt;I seem to remember reading somewhere that if MCUXpresso manages the peripherals that the clock configuration will stop edma from working.&lt;/P&gt;&lt;P&gt;If you are reading this and you are with NXP can you provide a reference on how to get this working with the config tool?&lt;/P&gt;</description>
    <pubDate>Fri, 15 Mar 2024 19:22:39 GMT</pubDate>
    <dc:creator>rantonetti</dc:creator>
    <dc:date>2024-03-15T19:22:39Z</dc:date>
    <item>
      <title>MCUXpresso eDMA use with LPI2C</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCUXpresso-eDMA-use-with-LPI2C/m-p/1829598#M135</link>
      <description>&lt;P&gt;This is a general question.&lt;/P&gt;&lt;P&gt;I have looked at the NXP provided edma slave board to board example project provided for the imxrt1050-evkb.&lt;/P&gt;&lt;P&gt;This project does not use the MCUXpresso peripheral configuration tool.&lt;/P&gt;&lt;P&gt;I have attempted to set the edma up for use with the lpi2c and I can't seem to get the edma working.&lt;/P&gt;&lt;P&gt;Is there a reason NXP did not enable the peripheral configuration tools for this demo?&lt;/P&gt;&lt;P&gt;It's seems as though all set up is done manually.&lt;/P&gt;&lt;P&gt;I seem to remember reading somewhere that if MCUXpresso manages the peripherals that the clock configuration will stop edma from working.&lt;/P&gt;&lt;P&gt;If you are reading this and you are with NXP can you provide a reference on how to get this working with the config tool?&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 19:22:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCUXpresso-eDMA-use-with-LPI2C/m-p/1829598#M135</guid>
      <dc:creator>rantonetti</dc:creator>
      <dc:date>2024-03-15T19:22:39Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso eDMA use with LPI2C</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCUXpresso-eDMA-use-with-LPI2C/m-p/1833232#M159</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205427"&gt;@rantonetti&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I wouldn't be able to say with certainty when (or if) the SDK team will fully implement the example codes with Peripherals Tool. But for now, the evkbimxrt1050_lpi2c_edma_b2b_transfer example projects, like the rest of the evkbimxrt1050 demos, are fully integrated with at least Pins and Clocks Tool.&lt;/P&gt;
&lt;P&gt;What errors do you see when setting up the eDMA on Peripherals Tool?&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Thu, 21 Mar 2024 22:28:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCUXpresso-eDMA-use-with-LPI2C/m-p/1833232#M159</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2024-03-21T22:28:07Z</dc:date>
    </item>
  </channel>
</rss>