<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic mcxn236 usb device mode without VBUS in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/mcxn236-usb-device-mode-without-VBUS/m-p/1910568#M1218</link>
    <description>&lt;P&gt;Hi NXP,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;We refer NXP SDK_2_14_0_FRDM-MCXN236_rfp USB device example to develop a USB device. However, is it possible to make the USB device mode work without VBUS?&lt;/P&gt;&lt;P&gt;If yes, how can we modify this in the SDK?&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Alan&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 17 Jul 2024 12:18:07 GMT</pubDate>
    <dc:creator>allu</dc:creator>
    <dc:date>2024-07-17T12:18:07Z</dc:date>
    <item>
      <title>mcxn236 usb device mode without VBUS</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/mcxn236-usb-device-mode-without-VBUS/m-p/1910568#M1218</link>
      <description>&lt;P&gt;Hi NXP,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;We refer NXP SDK_2_14_0_FRDM-MCXN236_rfp USB device example to develop a USB device. However, is it possible to make the USB device mode work without VBUS?&lt;/P&gt;&lt;P&gt;If yes, how can we modify this in the SDK?&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Alan&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jul 2024 12:18:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/mcxn236-usb-device-mode-without-VBUS/m-p/1910568#M1218</guid>
      <dc:creator>allu</dc:creator>
      <dc:date>2024-07-17T12:18:07Z</dc:date>
    </item>
    <item>
      <title>Re: mcxn236 usb device mode without VBUS</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/mcxn236-usb-device-mode-without-VBUS/m-p/1923673#M1428</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/233046"&gt;@allu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you very much for your patience.&lt;/P&gt;
&lt;P&gt;As I reviewed internally, please find below our feedback.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We strongly suggest customers to link MCX N2xx's USB_VBUS pin with USB connector as recommended in our&amp;nbsp; hardware design guide and&amp;nbsp; implemented in the official FRDM-MCX N 236 schematic.&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With the USB_VBUS pin detect, the application firmware can easily know&amp;nbsp; if the USB is attached or not.&lt;/P&gt;
&lt;P&gt;Leaving USB_VBUS&amp;nbsp; floating is possible, but require the software&amp;nbsp; skip the attach detection, and use a software state machine to check if the USB is linked or not. But we are not sure about the workload to implement this.&lt;/P&gt;
&lt;P&gt;Additonally, leaving USB_VBUS disconnect may impact on the USB certification attach and de-attach test, but it will not impact on other test items. As mentioned before, you may use the software approach to solve the attach and de-attach test item issue, but it is not our recommendation.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Anyway, we strongly suggest you to enable the USB_VBUS.&lt;/P&gt;
&lt;P&gt;Thank you,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Diego&lt;/P&gt;</description>
      <pubDate>Fri, 02 Aug 2024 06:02:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/mcxn236-usb-device-mode-without-VBUS/m-p/1923673#M1428</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2024-08-02T06:02:11Z</dc:date>
    </item>
  </channel>
</rss>