<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flash download in MCU Bootloader</title>
    <link>https://community.nxp.com/t5/MCU-Bootloader/Flash-download/m-p/912407#M964</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="344398" data-username="814420552@qq.com" href="https://community.nxp.com/people/814420552@qq.com"&gt;kui wu&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; What the board you are using? The official board or your own designed board?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; If it is your own designed board, do you make it works in the previous time?&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please also let me know your chip part number, when you download the code, the code also should related to your chip.&lt;/P&gt;&lt;P&gt;&amp;nbsp; If you have the JLINK, you can use the JLINK commander to check your board, can you find the ARM core or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Jul 2019 02:45:31 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2019-07-15T02:45:31Z</dc:date>
    <item>
      <title>Flash download</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/Flash-download/m-p/912406#M963</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/91065i73A0F921E6B9B53E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Hello， I got a problem when I&amp;nbsp; used ULINK to download code to flash, Can you give me some help?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/91066i81EB476E9B00C81E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and when i connect Freemaster it has one problem as the above screenshot, wish for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jul 2019 08:02:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/Flash-download/m-p/912406#M963</guid>
      <dc:creator>814420552</dc:creator>
      <dc:date>2019-07-12T08:02:11Z</dc:date>
    </item>
    <item>
      <title>Re: Flash download</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/Flash-download/m-p/912407#M964</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="344398" data-username="814420552@qq.com" href="https://community.nxp.com/people/814420552@qq.com"&gt;kui wu&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; What the board you are using? The official board or your own designed board?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; If it is your own designed board, do you make it works in the previous time?&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please also let me know your chip part number, when you download the code, the code also should related to your chip.&lt;/P&gt;&lt;P&gt;&amp;nbsp; If you have the JLINK, you can use the JLINK commander to check your board, can you find the ARM core or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jul 2019 02:45:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/Flash-download/m-p/912407#M964</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2019-07-15T02:45:31Z</dc:date>
    </item>
  </channel>
</rss>