<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KL27 connection via USB to KinetisFlashTool in MCU Bootloader</title>
    <link>https://community.nxp.com/t5/MCU-Bootloader/KL27-connection-via-USB-to-KinetisFlashTool/m-p/606411#M86</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The DOS command line tool BLHOST has worked on every PC.&lt;BR /&gt;&lt;BR /&gt;The Windows GUI tools works only on random PCs I've tried. :-(&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is something that the tool is assuming is present, perhaps a compiler DLL, that when is missing the tool does nothing.&lt;/P&gt;&lt;P&gt;No error, acts like it was never even started.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Sep 2016 14:40:57 GMT</pubDate>
    <dc:creator>bobpaddock</dc:creator>
    <dc:date>2016-09-19T14:40:57Z</dc:date>
    <item>
      <title>KL27 connection via USB to KinetisFlashTool</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/KL27-connection-via-USB-to-KinetisFlashTool/m-p/606409#M84</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have a KL27 soldered onto a custom USB board.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The new KinetisFlashTool won't connect directly to this chip via USB-HID, even though it shows up properly in the Device Manager as an HID device with the correct&amp;nbsp;VID and PID values.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is&amp;nbsp;the bootloader that ships inside each device supposed to connect to the KinetisFlashTool?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there some trick to get it to connect&amp;nbsp;the first time?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Sep 2016 18:31:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/KL27-connection-via-USB-to-KinetisFlashTool/m-p/606409#M84</guid>
      <dc:creator>brock</dc:creator>
      <dc:date>2016-09-09T18:31:38Z</dc:date>
    </item>
    <item>
      <title>Re: KL27 connection via USB to KinetisFlashTool</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/KL27-connection-via-USB-to-KinetisFlashTool/m-p/606410#M85</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We got this working by trying different WIN 7 machines until it started working with one.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Sep 2016 20:22:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/KL27-connection-via-USB-to-KinetisFlashTool/m-p/606410#M85</guid>
      <dc:creator>brock</dc:creator>
      <dc:date>2016-09-09T20:22:43Z</dc:date>
    </item>
    <item>
      <title>Re: KL27 connection via USB to KinetisFlashTool</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/KL27-connection-via-USB-to-KinetisFlashTool/m-p/606411#M86</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The DOS command line tool BLHOST has worked on every PC.&lt;BR /&gt;&lt;BR /&gt;The Windows GUI tools works only on random PCs I've tried. :-(&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is something that the tool is assuming is present, perhaps a compiler DLL, that when is missing the tool does nothing.&lt;/P&gt;&lt;P&gt;No error, acts like it was never even started.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Sep 2016 14:40:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/KL27-connection-via-USB-to-KinetisFlashTool/m-p/606411#M86</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2016-09-19T14:40:57Z</dc:date>
    </item>
  </channel>
</rss>