<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCU BootloaderのトピックS32K144 bootloader CAN and/or UART2</title>
    <link>https://community.nxp.com/t5/MCU-Bootloader/S32K144-bootloader-CAN-and-or-UART2/m-p/833982#M846</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;BR /&gt;I would need a bootloader code (or the rbf file) for the S32K144&amp;nbsp;MCU which works with CAN or UART2 (unfortunately I cannot use UART1, which is the only one used and working&amp;nbsp;with RAppID Tool).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there&amp;nbsp;an rbf file which is configured to use CAN communication or UART2?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thanks and kind regards,&lt;BR /&gt;Filippo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Aug 2018 10:32:00 GMT</pubDate>
    <dc:creator>filippo_malleo</dc:creator>
    <dc:date>2018-08-28T10:32:00Z</dc:date>
    <item>
      <title>S32K144 bootloader CAN and/or UART2</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/S32K144-bootloader-CAN-and-or-UART2/m-p/833982#M846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;BR /&gt;I would need a bootloader code (or the rbf file) for the S32K144&amp;nbsp;MCU which works with CAN or UART2 (unfortunately I cannot use UART1, which is the only one used and working&amp;nbsp;with RAppID Tool).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there&amp;nbsp;an rbf file which is configured to use CAN communication or UART2?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thanks and kind regards,&lt;BR /&gt;Filippo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Aug 2018 10:32:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/S32K144-bootloader-CAN-and-or-UART2/m-p/833982#M846</guid>
      <dc:creator>filippo_malleo</dc:creator>
      <dc:date>2018-08-28T10:32:00Z</dc:date>
    </item>
  </channel>
</rss>