<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCU Bootloader中的主题 Re: Does anybody have working example for K27 bootloader configuration area with changed USB strings?</title>
    <link>https://community.nxp.com/t5/MCU-Bootloader/Does-anybody-have-working-example-for-K27-bootloader/m-p/775242#M755</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mykhaylo Shcherbak&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You cannot change the USB String with the Bootloader Configuration Area.&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;The problem is that in order to execute ROM&amp;nbsp;bootloader, you need to reset the device,&lt;/SPAN&gt; and by reset the USB doesn't have access to flash, because it is the bus master 3, and &lt;SPAN class=""&gt;&lt;EM&gt;Flash Access Protection Register has "master 3 access protection" as 00&lt;/EM&gt;&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So you need to grant flash access to USB with &lt;SPAN class=""&gt;FMC-&amp;gt;PFAPR&lt;/SPAN&gt;, bus as you cannot modify the ROM bootloader, you are not able to modify the USB Strings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the inconveniences that this may cause you.&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Jan 2018 22:00:03 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2018-01-12T22:00:03Z</dc:date>
    <item>
      <title>Does anybody have working example for K27 bootloader configuration area with changed USB strings?</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/Does-anybody-have-working-example-for-K27-bootloader/m-p/775241#M754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'v tried as shown in attachments but VID/PID are changed but strings are default&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jan 2018 14:56:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/Does-anybody-have-working-example-for-K27-bootloader/m-p/775241#M754</guid>
      <dc:creator>mykhayloshcherb</dc:creator>
      <dc:date>2018-01-09T14:56:53Z</dc:date>
    </item>
    <item>
      <title>Re: Does anybody have working example for K27 bootloader configuration area with changed USB strings?</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/Does-anybody-have-working-example-for-K27-bootloader/m-p/775242#M755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mykhaylo Shcherbak&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You cannot change the USB String with the Bootloader Configuration Area.&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;The problem is that in order to execute ROM&amp;nbsp;bootloader, you need to reset the device,&lt;/SPAN&gt; and by reset the USB doesn't have access to flash, because it is the bus master 3, and &lt;SPAN class=""&gt;&lt;EM&gt;Flash Access Protection Register has "master 3 access protection" as 00&lt;/EM&gt;&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So you need to grant flash access to USB with &lt;SPAN class=""&gt;FMC-&amp;gt;PFAPR&lt;/SPAN&gt;, bus as you cannot modify the ROM bootloader, you are not able to modify the USB Strings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the inconveniences that this may cause you.&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jan 2018 22:00:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/Does-anybody-have-working-example-for-K27-bootloader/m-p/775242#M755</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2018-01-12T22:00:03Z</dc:date>
    </item>
  </channel>
</rss>