<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCU BootloaderのトピックMKV58F1 bootloader</title>
    <link>https://community.nxp.com/t5/MCU-Bootloader/MKV58F1-bootloader/m-p/772428#M750</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm looking at implementing firmware updates over an ethernet connection on a MKV58F1M. I can get my application to receive and store an update file into the internal flash. Is there a way to launch the bootloader such that it performs an update from a known location in the internal flash?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Apr 2018 15:40:32 GMT</pubDate>
    <dc:creator>eddwhite1</dc:creator>
    <dc:date>2018-04-06T15:40:32Z</dc:date>
    <item>
      <title>MKV58F1 bootloader</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/MKV58F1-bootloader/m-p/772428#M750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm looking at implementing firmware updates over an ethernet connection on a MKV58F1M. I can get my application to receive and store an update file into the internal flash. Is there a way to launch the bootloader such that it performs an update from a known location in the internal flash?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Apr 2018 15:40:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/MKV58F1-bootloader/m-p/772428#M750</guid>
      <dc:creator>eddwhite1</dc:creator>
      <dc:date>2018-04-06T15:40:32Z</dc:date>
    </item>
    <item>
      <title>Re: MKV58F1 bootloader</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/MKV58F1-bootloader/m-p/772429#M751</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In general, the bootloader routine located from internal Flash boot up address (0x0).&lt;/P&gt;&lt;P&gt;If there with suitable application code, after the chip boot up, the bootloader will jump to application code.&lt;/P&gt;&lt;P&gt;Customer could check &lt;A href="http://fnet.sourceforge.net/"&gt;here&lt;/A&gt; about Kinetis Ethernet bootloader demo for reference.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Apr 2018 06:52:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/MKV58F1-bootloader/m-p/772429#M751</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2018-04-09T06:52:51Z</dc:date>
    </item>
  </channel>
</rss>