<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCU BootloaderのトピックRunning Kinetis Flash Tool under VirtualBox (can't access USB or Serial)</title>
    <link>https://community.nxp.com/t5/MCU-Bootloader/Running-Kinetis-Flash-Tool-under-VirtualBox-can-t-access-USB-or/m-p/699516#M505</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'd like to run the Kinetis Flash Tool ("KFT") in order to compute CRCs for the Boot Control Area and all those other wonderful things that KFT can do.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I'm on a Mac, I need to run KFT under VirtualBox.&amp;nbsp; And I think my question is rather simple:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm connected to my FRDM-KL27Z board via USB on the Mac.&amp;nbsp; And I can access it as a serial device under /dev.cu.usbmodemNNN.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I launch&amp;nbsp;Kinetis Flash Tool under Virtualbox, I can't connect to the FRDM-KL27Z via USB or via Serial.&amp;nbsp; If I recall correctly, there's some special sequence you need to go through in order to get OS X to release the USB port so that the VirtualBox USB driver can connect them.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the short question is: how can I connect to the FRDM board from Kinetis Flash Tool running under VirtualBox?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Oct 2017 20:22:15 GMT</pubDate>
    <dc:creator>robertpoor</dc:creator>
    <dc:date>2017-10-05T20:22:15Z</dc:date>
    <item>
      <title>Running Kinetis Flash Tool under VirtualBox (can't access USB or Serial)</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/Running-Kinetis-Flash-Tool-under-VirtualBox-can-t-access-USB-or/m-p/699516#M505</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'd like to run the Kinetis Flash Tool ("KFT") in order to compute CRCs for the Boot Control Area and all those other wonderful things that KFT can do.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I'm on a Mac, I need to run KFT under VirtualBox.&amp;nbsp; And I think my question is rather simple:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm connected to my FRDM-KL27Z board via USB on the Mac.&amp;nbsp; And I can access it as a serial device under /dev.cu.usbmodemNNN.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I launch&amp;nbsp;Kinetis Flash Tool under Virtualbox, I can't connect to the FRDM-KL27Z via USB or via Serial.&amp;nbsp; If I recall correctly, there's some special sequence you need to go through in order to get OS X to release the USB port so that the VirtualBox USB driver can connect them.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the short question is: how can I connect to the FRDM board from Kinetis Flash Tool running under VirtualBox?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Oct 2017 20:22:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/Running-Kinetis-Flash-Tool-under-VirtualBox-can-t-access-USB-or/m-p/699516#M505</guid>
      <dc:creator>robertpoor</dc:creator>
      <dc:date>2017-10-05T20:22:15Z</dc:date>
    </item>
    <item>
      <title>Re: Running Kinetis Flash Tool under VirtualBox (can't access USB or Serial)</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/Running-Kinetis-Flash-Tool-under-VirtualBox-can-t-access-USB-or/m-p/699517#M506</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually I have never try to run the KFT on an Mac OS. And I remembered that the Mac OS is quite different with others even run with a VirturalBox. (not sure the real reason). You may would like to see this post:&lt;A _jive_internal="true" class="jivelink10" href="https://community.nxp.com/thread/440033" title="https://community.nxp.com/thread/440033"&gt;https://community.nxp.com/thread/440033. &lt;/A&gt;&lt;/P&gt;&lt;P&gt;So would you mind to change another Macbook to try? Does the problem still exist?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Oct 2017 07:12:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/Running-Kinetis-Flash-Tool-under-VirtualBox-can-t-access-USB-or/m-p/699517#M506</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2017-10-11T07:12:10Z</dc:date>
    </item>
    <item>
      <title>Re: Running Kinetis Flash Tool under VirtualBox (can't access USB or Serial)</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/Running-Kinetis-Flash-Tool-under-VirtualBox-can-t-access-USB-or/m-p/699518#M507</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I have never try to run the KFT on an Mac OS.&amp;nbsp; ... would you mind to change to another Macbook?&lt;/SPAN&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I am confused: is it possible to run the KFT&amp;nbsp;on Mac OS X?&amp;nbsp; To the best of my understanding, KFT only runs under Windows.&amp;nbsp; This is why I was trying to run KFT under VirtualBox.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The link you included (&lt;A _jive_internal="true" class="jivelink11" href="https://community.nxp.com/thread/440033" title="https://community.nxp.com/thread/440033"&gt;https://community.nxp.com/thread/440033&lt;/A&gt;) is about running KDS and JLink under OS X -- I do that all the time and have no problem with it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you suggesting that KFT is included as a part of KDS?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please clarify?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Oct 2017 11:34:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/Running-Kinetis-Flash-Tool-under-VirtualBox-can-t-access-USB-or/m-p/699518#M507</guid>
      <dc:creator>robertpoor</dc:creator>
      <dc:date>2017-10-11T11:34:14Z</dc:date>
    </item>
  </channel>
</rss>