<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic eraseRegion min/max eraseable bytes in MCU Bootloader</title>
    <link>https://community.nxp.com/t5/MCU-Bootloader/eraseRegion-min-max-eraseable-bytes/m-p/697432#M472</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the bootloader to erase Flash with the eraseRegion command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How big/small is the byte-count that i can use? Do i have to make shure the byteCount fits in the page-size?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using a "MK02FN64VLH10".&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Sep 2017 09:36:10 GMT</pubDate>
    <dc:creator>albrecht</dc:creator>
    <dc:date>2017-09-07T09:36:10Z</dc:date>
    <item>
      <title>eraseRegion min/max eraseable bytes</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/eraseRegion-min-max-eraseable-bytes/m-p/697432#M472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the bootloader to erase Flash with the eraseRegion command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How big/small is the byte-count that i can use? Do i have to make shure the byteCount fits in the page-size?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using a "MK02FN64VLH10".&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Sep 2017 09:36:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/eraseRegion-min-max-eraseable-bytes/m-p/697432#M472</guid>
      <dc:creator>albrecht</dc:creator>
      <dc:date>2017-09-07T09:36:10Z</dc:date>
    </item>
    <item>
      <title>Re: eraseRegion min/max eraseable bytes</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/eraseRegion-min-max-eraseable-bytes/m-p/697433#M473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Flash is erased on sector boundaries. For MK02, the minimum erase size is 4K bytes (one sector of program flash). So the eraseRegion min eraseable bytes is 4K.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Sep 2017 07:15:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/eraseRegion-min-max-eraseable-bytes/m-p/697433#M473</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2017-09-13T07:15:26Z</dc:date>
    </item>
  </channel>
</rss>