<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic KL03 bootloader DLL? in MCU Bootloader</title>
    <link>https://community.nxp.com/t5/MCU-Bootloader/KL03-bootloader-DLL/m-p/678422#M382</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm preparing for a KL03 design from our product dev group and I'm the guy who gets the production tools done.&amp;nbsp; We will be programming the uP in a production environment and from what I've found the serial boot loader is the way to go.&amp;nbsp; I will have a custom designed PCB for testing the product and I can easily add a serial port that the PC can use to program the KL03 directly but to do that I'd need a bootloader DLL and associated API documentation to make a PC app that talks to our internal database for programming parameters.&amp;nbsp; The other way is to code the boot loader into the uP on my custom PCB using the low level bootloader protocol documentation and use it to program the KL03.&amp;nbsp; The PC option would be much easier.&amp;nbsp; Is the DLL and API reference available and if so, where would I find it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Jun 2017 14:07:13 GMT</pubDate>
    <dc:creator>andrewbarnes</dc:creator>
    <dc:date>2017-06-07T14:07:13Z</dc:date>
    <item>
      <title>KL03 bootloader DLL?</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/KL03-bootloader-DLL/m-p/678422#M382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm preparing for a KL03 design from our product dev group and I'm the guy who gets the production tools done.&amp;nbsp; We will be programming the uP in a production environment and from what I've found the serial boot loader is the way to go.&amp;nbsp; I will have a custom designed PCB for testing the product and I can easily add a serial port that the PC can use to program the KL03 directly but to do that I'd need a bootloader DLL and associated API documentation to make a PC app that talks to our internal database for programming parameters.&amp;nbsp; The other way is to code the boot loader into the uP on my custom PCB using the low level bootloader protocol documentation and use it to program the KL03.&amp;nbsp; The PC option would be much easier.&amp;nbsp; Is the DLL and API reference available and if so, where would I find it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2017 14:07:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/KL03-bootloader-DLL/m-p/678422#M382</guid>
      <dc:creator>andrewbarnes</dc:creator>
      <dc:date>2017-06-07T14:07:13Z</dc:date>
    </item>
    <item>
      <title>Re: KL03 bootloader DLL?</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/KL03-bootloader-DLL/m-p/678423#M383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KL03 chip provides the ROM bootloader.&lt;/P&gt;&lt;P&gt;NXP provides the Kinetis Flash Tool, which is a GUI application on Windows® OS, aiming to offer the user an ease-of-use friendly user interface to communicate with the Kinetis device, running the Kinetis bootloader application.&lt;/P&gt;&lt;P&gt;This tool Supports Kinetis devices with Kinetis ROM bootloader, Kinetis flashloader, or running the flash resident&lt;BR /&gt;bootloader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Customer could get this tool at [NXP_Kinetis_Bootloader_2.0.0 package] software, which could be downloaded from &lt;A href="http://www.nxp.com/products/reference-designs/kinetis-bootloader:KBOOT?tab=Design_Tools_Tab"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;The &amp;lt;Kinetis Flash Tool User's Guide&amp;gt; could be found with below path:&lt;/P&gt;&lt;P&gt;..\NXP_Kinetis_Bootloader_2_0_0\doc&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2017 08:22:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/KL03-bootloader-DLL/m-p/678423#M383</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-06-13T08:22:38Z</dc:date>
    </item>
  </channel>
</rss>