<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCU Bootloader中的主题 Bootloader (MSC) doesn't load BIN</title>
    <link>https://community.nxp.com/t5/MCU-Bootloader/Bootloader-MSC-doesn-t-load-BIN/m-p/659048#M337</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;K64F Freedom board, bootloader 2.0, MSC usage.&lt;BR /&gt;I built the bootloader with HID and MSC only enabled devices, with BL_APP_VECTOR_TABLE_ADDRESS 0xa000.&lt;BR /&gt;Updated the project to generate a BIN file and dragged it onto the MBED MSC loader to install it.&lt;/P&gt;&lt;P&gt;I connect the K64F USB to the host and see the expected window to drop BIN image, including the STATUS.TXT file.&lt;/P&gt;&lt;P&gt;So, looks like the bootloader built OK and is running OK.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I drag the LED demo file onto this window, nothing happens except the filename is added to the directory:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="166353_166353.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/122391iBD671E5144DC305D/image-size/large?v=v2&amp;amp;px=999" role="button" title="166353_166353.PNG" alt="166353_166353.PNG" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Bootloader_doesn't_load.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6494i0A37822CBF135B93/image-size/large?v=v2&amp;amp;px=999" role="button" title="Bootloader_doesn't_load.PNG" alt="Bootloader_doesn't_load.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If I launch the LED test application via the debugger it does indeed blink the LED.&lt;/P&gt;&lt;P&gt;The LD file for the LED blink looks correctly set to start at 0xA000, matching the bootloader.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance for any assistance,&lt;BR /&gt;Best Regards, Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Oct 2016 20:11:41 GMT</pubDate>
    <dc:creator>davenadler</dc:creator>
    <dc:date>2016-10-21T20:11:41Z</dc:date>
    <item>
      <title>Bootloader (MSC) doesn't load BIN</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/Bootloader-MSC-doesn-t-load-BIN/m-p/659048#M337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;K64F Freedom board, bootloader 2.0, MSC usage.&lt;BR /&gt;I built the bootloader with HID and MSC only enabled devices, with BL_APP_VECTOR_TABLE_ADDRESS 0xa000.&lt;BR /&gt;Updated the project to generate a BIN file and dragged it onto the MBED MSC loader to install it.&lt;/P&gt;&lt;P&gt;I connect the K64F USB to the host and see the expected window to drop BIN image, including the STATUS.TXT file.&lt;/P&gt;&lt;P&gt;So, looks like the bootloader built OK and is running OK.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I drag the LED demo file onto this window, nothing happens except the filename is added to the directory:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="166353_166353.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/122391iBD671E5144DC305D/image-size/large?v=v2&amp;amp;px=999" role="button" title="166353_166353.PNG" alt="166353_166353.PNG" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Bootloader_doesn't_load.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6494i0A37822CBF135B93/image-size/large?v=v2&amp;amp;px=999" role="button" title="Bootloader_doesn't_load.PNG" alt="Bootloader_doesn't_load.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If I launch the LED test application via the debugger it does indeed blink the LED.&lt;/P&gt;&lt;P&gt;The LD file for the LED blink looks correctly set to start at 0xA000, matching the bootloader.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance for any assistance,&lt;BR /&gt;Best Regards, Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Oct 2016 20:11:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/Bootloader-MSC-doesn-t-load-BIN/m-p/659048#M337</guid>
      <dc:creator>davenadler</dc:creator>
      <dc:date>2016-10-21T20:11:41Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader (MSC) doesn't load BIN</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/Bootloader-MSC-doesn-t-load-BIN/m-p/659049#M338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Whoops, the bootloader 2.0 MSC only supports the "SB" secure-binary format (unlike the mbed loader).&lt;BR /&gt;Documented in a corner of the bootloader reference manual, aaarrgggg.....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP: This question has come up many times on this forum - It would be great if this was &lt;STRONG style="text-decoration: underline;"&gt;prominently&lt;/STRONG&gt; explained in the documentation!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Oct 2016 22:12:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/Bootloader-MSC-doesn-t-load-BIN/m-p/659049#M338</guid>
      <dc:creator>davenadler</dc:creator>
      <dc:date>2016-10-21T22:12:20Z</dc:date>
    </item>
  </channel>
</rss>