<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCU BootloaderのトピックDoes the ROM Bootloader in the KL27 support RS485 loading of firmware?</title>
    <link>https://community.nxp.com/t5/MCU-Bootloader/Does-the-ROM-Bootloader-in-the-KL27-support-RS485-loading-of/m-p/635040#M235</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there. I hope this question has not been solved elsewhere. I have a customer who is looking at the KL27 which has the boot loader in ROM and would like the ability to re-flash the device over RS485 instead of serial. Will the boot loader and flashing tool support this provided that the UART to RS485 transceiver has an automatic direction setup? I know with a soft boot loader it can be done and I have seen it mentioned in a few places however I do not see any mention of the parts with the boot loader in ROM.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Mar 2017 00:33:56 GMT</pubDate>
    <dc:creator>paulmerana</dc:creator>
    <dc:date>2017-03-09T00:33:56Z</dc:date>
    <item>
      <title>Does the ROM Bootloader in the KL27 support RS485 loading of firmware?</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/Does-the-ROM-Bootloader-in-the-KL27-support-RS485-loading-of/m-p/635040#M235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there. I hope this question has not been solved elsewhere. I have a customer who is looking at the KL27 which has the boot loader in ROM and would like the ability to re-flash the device over RS485 instead of serial. Will the boot loader and flashing tool support this provided that the UART to RS485 transceiver has an automatic direction setup? I know with a soft boot loader it can be done and I have seen it mentioned in a few places however I do not see any mention of the parts with the boot loader in ROM.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Mar 2017 00:33:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/Does-the-ROM-Bootloader-in-the-KL27-support-RS485-loading-of/m-p/635040#M235</guid>
      <dc:creator>paulmerana</dc:creator>
      <dc:date>2017-03-09T00:33:56Z</dc:date>
    </item>
    <item>
      <title>Re: Does the ROM Bootloader in the KL27 support RS485 loading of firmware?</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/Does-the-ROM-Bootloader-in-the-KL27-support-RS485-loading-of/m-p/635041#M236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paul Merana,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; No, the KL27 ROM bootloader can't support the RS485 loading firmware now.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Just as you said, RS485 need to control /RE and DE pin, but the KL27 ROM just support the UART, two pin communication pin, no direction control pin now.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; So, if you want to use the RS485 to load the App code, you need to use the flash bootloader and add the according 485 direction control code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please let me know!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;(my name)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Mar 2017 05:59:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/Does-the-ROM-Bootloader-in-the-KL27-support-RS485-loading-of/m-p/635041#M236</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-03-15T05:59:01Z</dc:date>
    </item>
    <item>
      <title>Re: Does the ROM Bootloader in the KL27 support RS485 loading of firmware?</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/Does-the-ROM-Bootloader-in-the-KL27-support-RS485-loading-of/m-p/635042#M237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the reply. The problem really is not the /RE DE lines as the hardware can be set up for auto direction control similar to the circuit in the link.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.seekic.com/uploadfile/ic-circuit/s201152772159916.gif" title="http://www.seekic.com/uploadfile/ic-circuit/s201152772159916.gif"&gt;http://www.seekic.com/uploadfile/ic-circuit/s201152772159916.gif&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem would be the traffic timing. Is it purely half duplex or does it need full duplex communications ability?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Mar 2017 13:19:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/Does-the-ROM-Bootloader-in-the-KL27-support-RS485-loading-of/m-p/635042#M237</guid>
      <dc:creator>paulmerana</dc:creator>
      <dc:date>2017-03-15T13:19:30Z</dc:date>
    </item>
    <item>
      <title>Re: Does the ROM Bootloader in the KL27 support RS485 loading of firmware?</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/Does-the-ROM-Bootloader-in-the-KL27-support-RS485-loading-of/m-p/635043#M238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paul Merana,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; If your auto direction control circuit can meet the UART baud rate, of course you can use it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; You need to adjust the traffic timing, for example, baud rate is 115200, your time should follow it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; The uart is half duplex communications.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Maybe you can try to find a 485 chip which has the auto control function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P style="padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Mar 2017 07:20:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/Does-the-ROM-Bootloader-in-the-KL27-support-RS485-loading-of/m-p/635043#M238</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-03-16T07:20:27Z</dc:date>
    </item>
  </channel>
</rss>