<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Peripheral Detection Timeout with direct call rom bootloader in MCU Bootloader</title>
    <link>https://community.nxp.com/t5/MCU-Bootloader/Peripheral-Detection-Timeout-with-direct-call-rom-bootloader/m-p/1662672#M1391</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;is there a way to enable the Peripheral Detection Timeout defined in BCA with direct call to bootloader? It seems if I call the runBootloader function than the timeout is disabled. Maybe there is a way like the passed argument or something else.&lt;/P&gt;&lt;P&gt;Thanks a lot in advance&lt;/P&gt;</description>
    <pubDate>Fri, 02 Jun 2023 12:47:54 GMT</pubDate>
    <dc:creator>nobodyKnows</dc:creator>
    <dc:date>2023-06-02T12:47:54Z</dc:date>
    <item>
      <title>Peripheral Detection Timeout with direct call rom bootloader</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/Peripheral-Detection-Timeout-with-direct-call-rom-bootloader/m-p/1662672#M1391</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;is there a way to enable the Peripheral Detection Timeout defined in BCA with direct call to bootloader? It seems if I call the runBootloader function than the timeout is disabled. Maybe there is a way like the passed argument or something else.&lt;/P&gt;&lt;P&gt;Thanks a lot in advance&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jun 2023 12:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/Peripheral-Detection-Timeout-with-direct-call-rom-bootloader/m-p/1662672#M1391</guid>
      <dc:creator>nobodyKnows</dc:creator>
      <dc:date>2023-06-02T12:47:54Z</dc:date>
    </item>
    <item>
      <title>Re: Peripheral Detection Timeout with direct call rom bootloader</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/Peripheral-Detection-Timeout-with-direct-call-rom-bootloader/m-p/1663651#M1394</link>
      <description>&lt;P&gt;Hello, could you tell me what kind of target are you using?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Mon, 05 Jun 2023 17:50:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/Peripheral-Detection-Timeout-with-direct-call-rom-bootloader/m-p/1663651#M1394</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-06-05T17:50:41Z</dc:date>
    </item>
  </channel>
</rss>