<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCUBOOT / Application - problem with SPI interface in MCU Bootloader</title>
    <link>https://community.nxp.com/t5/MCU-Bootloader/MCUBOOT-Application-problem-with-SPI-interface/m-p/971900#M1061</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Allen,&lt;/P&gt;&lt;P&gt;1. What do you mean of crash, hardfault? The only situation I can image is the SPI peripheral clock isn't set.&lt;/P&gt;&lt;P&gt;2. No, it couldn't. These application is base on the driver. If the SPI is initialized well, is won't cause crash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Aug 2019 07:27:21 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2019-08-27T07:27:21Z</dc:date>
    <item>
      <title>MCUBOOT / Application - problem with SPI interface</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/MCUBOOT-Application-problem-with-SPI-interface/m-p/971899#M1060</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have system that is using a K22FN512 as a SPI slave to a K61 master.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K61 is meant to communicate to the K22 through SPI - for normal operation and also for loading new application firmware into the K22.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I am seeing is that if the application is loaded normally, without a bootloader,&amp;nbsp;the K61 and K22 can communicate.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the K22 application is loaded by the bootloader - the application call to:&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;DSPI_FlushFifo &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt; base&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; true&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; true &lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;within the&amp;nbsp;&lt;SPAN&gt;DSPI_SlaveTransferNonBlocking() function will crash.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I change&amp;nbsp;DSPI_SlaveTransferNonBlocking() to use:&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;DSPI_FlushFifo &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt; base&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; false&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; true &lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;  &lt;SPAN class="comment token"&gt;// don't flush the TX FIFO‍&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;the K22 application will not crash - but it also doesn't respond to the master.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In this state the K22 is still able to receive data from the K61 but I don't see anything coming from the K22 (verified with an oscilloscope).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The&amp;nbsp;DSPI_FlushFifo() function just sets a couple of bits in the MCR register:&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="comment token"&gt;/*!
 * @brief Flushes the DSPI FIFOs.
 *
 * @param base DSPI peripheral address.
 * @param flushTxFifo Flushes (true) the Tx FIFO; Otherwise, does not flush (false) the Tx FIFO
 * @param flushRxFifo Flushes (true) the Rx FIFO; Otherwise, does not flush (false) the Rx FIFO
 */&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;inline&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;DSPI_FlushFifo&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;SPI_Type &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;base&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; bool flushTxFifo&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; bool flushRxFifo&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 base&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;MCR &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;base&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;MCR &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;~&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;SPI_MCR_CLR_TXF_MASK &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; SPI_MCR_CLR_RXF_MASK&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;
 &lt;SPAN class="token function"&gt;SPI_MCR_CLR_TXF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;true &lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt; flushTxFifo &lt;SPAN class="operator token"&gt;?&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1U&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0U&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;SPI_MCR_CLR_RXF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;true &lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt; flushRxFifo &lt;SPAN class="operator token"&gt;?&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1U&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0U&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;‍‍‍‍‍‍‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Under what conditions could setting the CLR_TXF bit in the MCR register cause a problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) Could the MCU bootloader be leaving the SPI peripheral in a state that&amp;nbsp;DSPI_SlaveTransferNonBlocking() isn't expecting?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;MCUXpresso IDE v11.0.0&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;SDK 2.6.0&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;MCUBOOT 2.7.0&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Aug 2019 19:53:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/MCUBOOT-Application-problem-with-SPI-interface/m-p/971899#M1060</guid>
      <dc:creator>gorakk</dc:creator>
      <dc:date>2019-08-26T19:53:28Z</dc:date>
    </item>
    <item>
      <title>Re: MCUBOOT / Application - problem with SPI interface</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/MCUBOOT-Application-problem-with-SPI-interface/m-p/971900#M1061</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Allen,&lt;/P&gt;&lt;P&gt;1. What do you mean of crash, hardfault? The only situation I can image is the SPI peripheral clock isn't set.&lt;/P&gt;&lt;P&gt;2. No, it couldn't. These application is base on the driver. If the SPI is initialized well, is won't cause crash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2019 07:27:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/MCUBOOT-Application-problem-with-SPI-interface/m-p/971900#M1061</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-08-27T07:27:21Z</dc:date>
    </item>
  </channel>
</rss>