<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCU BootloaderのトピックRe: MPC5746C Bootloader with MPC574XG-MB DEVKIT</title>
    <link>https://community.nxp.com/t5/MCU-Bootloader/MPC5746C-Bootloader-with-MPC574XG-MB-DEVKIT/m-p/965097#M1045</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;rbf file for MPC5746C can be found in this package:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=RAPPID_BOOTLOADER_UTILITY&amp;amp;appType=license" title="https://www.nxp.com/webapp/Download?colCode=RAPPID_BOOTLOADER_UTILITY&amp;amp;appType=license"&gt;https://www.nxp.com/webapp/Download?colCode=RAPPID_BOOTLOADER_UTILITY&amp;amp;appType=license&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, just connect USB cable to MPC574xG-MB. You can test which COM port it is - two new port should appear.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Don't do power-off / power-on sequence as suggested by the message, just reset the MCU by button. Power cycling can't be used due to serial-to-USB bridge.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There's relatively small delay, so try to reset the MCU and then click on "Start Bootloader" in about 1s or less. This was working on my side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Jul 2019 06:13:08 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2019-07-10T06:13:08Z</dc:date>
    <item>
      <title>MPC5746C Bootloader with MPC574XG-MB DEVKIT</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/MPC5746C-Bootloader-with-MPC574XG-MB-DEVKIT/m-p/965096#M1044</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using S32 DS, SDK RTM v3.0.0 with MPC574XG devkit and MPC5746C MCU.&lt;BR /&gt;I've searched a lot of documents and discussion regarding this issue but I cannot find any document that explains clearly for the bootloader via RAppID.&lt;BR /&gt;My goal is to develop a bootloader for MPC5746C MCU Meanwhile there is an example for the MPC5748G and I have got an MPC5748G MCU. I applied every stage that explains description path of the example project but when I try to download the .srec file via RAppID program, a classic error occurred like the following image Loss Communication CCP MCU! Some thread mentioned about this problem but nobody has shared a good solution or sample project exactly!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/89575i194A8833C7917273/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&amp;nbsp; &amp;nbsp;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/89576i552032E80429AA11/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My questions are:&lt;/P&gt;&lt;P&gt;1-&amp;nbsp; I need an MPC5746C "RBF" file, where can I find it?&lt;/P&gt;&lt;P&gt;2-&amp;nbsp; How can I connect the DEVKIT board serial port correctly? Only needs to connect with a serial USB cable?&lt;/P&gt;&lt;P&gt;3-&amp;nbsp; How can I fix this CCP MCU error? What is the root cause?&amp;nbsp;&lt;/P&gt;&lt;P&gt;4-&amp;nbsp; There are some RBF file in the "MBDToolbox_MPC57xx_3.0.0_20190218"&amp;nbsp; folder. Can I use this RBF file for general usage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jun 2019 13:32:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/MPC5746C-Bootloader-with-MPC574XG-MB-DEVKIT/m-p/965096#M1044</guid>
      <dc:creator>eyupozer</dc:creator>
      <dc:date>2019-06-24T13:32:57Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5746C Bootloader with MPC574XG-MB DEVKIT</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/MPC5746C-Bootloader-with-MPC574XG-MB-DEVKIT/m-p/965097#M1045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;rbf file for MPC5746C can be found in this package:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=RAPPID_BOOTLOADER_UTILITY&amp;amp;appType=license" title="https://www.nxp.com/webapp/Download?colCode=RAPPID_BOOTLOADER_UTILITY&amp;amp;appType=license"&gt;https://www.nxp.com/webapp/Download?colCode=RAPPID_BOOTLOADER_UTILITY&amp;amp;appType=license&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, just connect USB cable to MPC574xG-MB. You can test which COM port it is - two new port should appear.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Don't do power-off / power-on sequence as suggested by the message, just reset the MCU by button. Power cycling can't be used due to serial-to-USB bridge.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There's relatively small delay, so try to reset the MCU and then click on "Start Bootloader" in about 1s or less. This was working on my side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jul 2019 06:13:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/MPC5746C-Bootloader-with-MPC574XG-MB-DEVKIT/m-p/965097#M1045</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2019-07-10T06:13:08Z</dc:date>
    </item>
  </channel>
</rss>