<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Bootloader MC9S12E128 in MCU Bootloader</title>
    <link>https://community.nxp.com/t5/MCU-Bootloader/Bootloader-MC9S12E128/m-p/952538#M1024</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;there we a few bootloaders written in history - yr.2005 and older.&lt;/P&gt;&lt;P&gt;I have attached , I think, al of them.&lt;/P&gt;&lt;P&gt;1) The first set contains similar approaches but I am not sure they are absolute clear. AN2153, AN2546&lt;/P&gt;&lt;P&gt;2) The bootloader I prefer to port to E128 device is AN3275&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note; the bootloaders 1) use linear format of S19 record so if you have Page_offset format of the S19 record form CodeWarrior you have to transform it to linear format. Bootloader 2) is able to useS19 record directly generated from CodeWarior. &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Linear format can be get by means of SreCvt program.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is really good to study principle of the bootloader and test all routines step by step to understand it and to avoid any mistake.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition, only as an example of evolution in the family, I have also attache bootloader for S12P,G,XE devices AN4258.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Jul 2019 06:45:00 GMT</pubDate>
    <dc:creator>lama</dc:creator>
    <dc:date>2019-07-23T06:45:00Z</dc:date>
    <item>
      <title>Bootloader MC9S12E128</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/Bootloader-MC9S12E128/m-p/952537#M1023</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need a bootloader for MC9S12E128.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jul 2019 08:17:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/Bootloader-MC9S12E128/m-p/952537#M1023</guid>
      <dc:creator>lucatollot</dc:creator>
      <dc:date>2019-07-22T08:17:38Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader MC9S12E128</title>
      <link>https://community.nxp.com/t5/MCU-Bootloader/Bootloader-MC9S12E128/m-p/952538#M1024</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;there we a few bootloaders written in history - yr.2005 and older.&lt;/P&gt;&lt;P&gt;I have attached , I think, al of them.&lt;/P&gt;&lt;P&gt;1) The first set contains similar approaches but I am not sure they are absolute clear. AN2153, AN2546&lt;/P&gt;&lt;P&gt;2) The bootloader I prefer to port to E128 device is AN3275&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note; the bootloaders 1) use linear format of S19 record so if you have Page_offset format of the S19 record form CodeWarrior you have to transform it to linear format. Bootloader 2) is able to useS19 record directly generated from CodeWarior. &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Linear format can be get by means of SreCvt program.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is really good to study principle of the bootloader and test all routines step by step to understand it and to avoid any mistake.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition, only as an example of evolution in the family, I have also attache bootloader for S12P,G,XE devices AN4258.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ladislav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jul 2019 06:45:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCU-Bootloader/Bootloader-MC9S12E128/m-p/952538#M1024</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2019-07-23T06:45:00Z</dc:date>
    </item>
  </channel>
</rss>