<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Does LS1028A processor support the “half QSGMII” feature required by VSC8562-11 QSGMII PHY? in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Does-LS1028A-processor-support-the-half-QSGMII-feature-required/m-p/1406953#M9966</link>
    <description>&lt;P&gt;In our project we are interfacing VSC8562-11 QSGMII PHY to the LS1028A processor's TSN switch SerDes port.&lt;/P&gt;&lt;P&gt;VSC8562-11 is a Dual-Port 10/100/1000BASE-T PHY and in its datasheet we observed as follows:&amp;nbsp;&lt;/P&gt;&lt;P&gt;Two of the four QSGMII channels contain data. The windows for the other two channels remain present&lt;BR /&gt;and need to be supported in both directions by the MAC. This support is called “half QSGMII.”&lt;/P&gt;&lt;P&gt;Can you please confirm me that LS1028A processor supports this&amp;nbsp;“half QSGMII” feature?&lt;/P&gt;</description>
    <pubDate>Mon, 31 Jan 2022 07:56:23 GMT</pubDate>
    <dc:creator>Nithya</dc:creator>
    <dc:date>2022-01-31T07:56:23Z</dc:date>
    <item>
      <title>Does LS1028A processor support the “half QSGMII” feature required by VSC8562-11 QSGMII PHY?</title>
      <link>https://community.nxp.com/t5/Layerscape/Does-LS1028A-processor-support-the-half-QSGMII-feature-required/m-p/1406953#M9966</link>
      <description>&lt;P&gt;In our project we are interfacing VSC8562-11 QSGMII PHY to the LS1028A processor's TSN switch SerDes port.&lt;/P&gt;&lt;P&gt;VSC8562-11 is a Dual-Port 10/100/1000BASE-T PHY and in its datasheet we observed as follows:&amp;nbsp;&lt;/P&gt;&lt;P&gt;Two of the four QSGMII channels contain data. The windows for the other two channels remain present&lt;BR /&gt;and need to be supported in both directions by the MAC. This support is called “half QSGMII.”&lt;/P&gt;&lt;P&gt;Can you please confirm me that LS1028A processor supports this&amp;nbsp;“half QSGMII” feature?&lt;/P&gt;</description>
      <pubDate>Mon, 31 Jan 2022 07:56:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Does-LS1028A-processor-support-the-half-QSGMII-feature-required/m-p/1406953#M9966</guid>
      <dc:creator>Nithya</dc:creator>
      <dc:date>2022-01-31T07:56:23Z</dc:date>
    </item>
    <item>
      <title>Re: Does LS1028A processor support the “half QSGMII” feature required by VSC8562-11 QSGMII PHY?</title>
      <link>https://community.nxp.com/t5/Layerscape/Does-LS1028A-processor-support-the-half-QSGMII-feature-required/m-p/1406985#M9967</link>
      <description>&lt;P&gt;LS1028A supports QSGMII.&lt;/P&gt;&lt;P&gt;According to the PHY datasheet it also supports QSGMII, so physical interface should work.&lt;/P&gt;&lt;P&gt;&amp;gt; Can you please confirm me that LS1028A processor supports this “half QSGMII” feature?&lt;/P&gt;&lt;P&gt;The feature was not tested, but using two MACs of available four should not introduce a trouble.&lt;/P&gt;</description>
      <pubDate>Mon, 31 Jan 2022 09:28:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Does-LS1028A-processor-support-the-half-QSGMII-feature-required/m-p/1406985#M9967</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2022-01-31T09:28:59Z</dc:date>
    </item>
  </channel>
</rss>