<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LX2160ARDB_REV2 SFP RX Issue</title>
    <link>https://community.nxp.com/t5/Layerscape/LX2160ARDB-REV2-SFP-RX-Issue/m-p/1404221#M9923</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Please check the attachments.&lt;/P&gt;&lt;P&gt;Including uboot log, serdes1-sch and clockgen-sch.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 25 Jan 2022 01:38:10 GMT</pubDate>
    <dc:creator>tsungmin_wang</dc:creator>
    <dc:date>2022-01-25T01:38:10Z</dc:date>
    <item>
      <title>LX2160ARDB_REV2 SFP RX Issue</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160ARDB-REV2-SFP-RX-Issue/m-p/1403863#M9919</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;We use XFI to connect to SFP cage without PHY.&lt;/P&gt;&lt;P&gt;Currently, the system can detect the link status of SFP cage.&lt;/P&gt;&lt;P&gt;But, when I used pktgen to test. I found that the receive side could not get any packet.&lt;/P&gt;&lt;P&gt;I just connected the SFP port directly.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="tmp.drawio.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/168612i0391B7225CE89402/image-size/medium?v=v2&amp;amp;px=400" role="button" title="tmp.drawio.png" alt="tmp.drawio.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;tmp.drawio.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;And make sure the status&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="tsungmin_wang_0-1643014884758.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/168613i3467E3C88FE65A23/image-size/medium?v=v2&amp;amp;px=400" role="button" title="tsungmin_wang_0-1643014884758.png" alt="tsungmin_wang_0-1643014884758.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;tsungmin_wang_0-1643014884758.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;ifconfig after pktgen&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;eth8: flags=4163&amp;lt;UP,BROADCAST,RUNNING,MULTICAST&amp;gt;  mtu 1500
        inet6 fe80::b8fe:9ff:fe4f:1c4e  prefixlen 64  scopeid 0x20&amp;lt;link&amp;gt;
        ether ba:fe:09:4f:1c:4e  txqueuelen 1000  (Ethernet)
        RX packets 0  bytes 0 (0.0 B)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 1010  bytes 58796 (57.4 KiB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

eth9: flags=4163&amp;lt;UP,BROADCAST,RUNNING,MULTICAST&amp;gt;  mtu 1500
        inet6 fe80::2044:c6ff:febd:e856  prefixlen 64  scopeid 0x20&amp;lt;link&amp;gt;
        ether 22:44:c6:bd:e8:56  txqueuelen 1000  (Ethernet)
        RX packets 0  bytes 0 (0.0 B)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 10  bytes 796 (796.0 B)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;RX packets of the receive side (eth9) is still 0, what may cause this issue?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jan 2022 09:06:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160ARDB-REV2-SFP-RX-Issue/m-p/1403863#M9919</guid>
      <dc:creator>tsungmin_wang</dc:creator>
      <dc:date>2022-01-24T09:06:43Z</dc:date>
    </item>
    <item>
      <title>Re: LX2160ARDB_REV2 SFP RX Issue</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160ARDB-REV2-SFP-RX-Issue/m-p/1404122#M9922</link>
      <description>&lt;P&gt;Please provide additional information:&lt;/P&gt;&lt;P&gt;1) U-Boot booting log&lt;/P&gt;&lt;P&gt;2) the processor connection schematics&lt;/P&gt;&lt;P&gt;3) frequencies of all applied SerDes reference clocks&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jan 2022 18:17:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160ARDB-REV2-SFP-RX-Issue/m-p/1404122#M9922</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2022-01-24T18:17:57Z</dc:date>
    </item>
    <item>
      <title>Re: LX2160ARDB_REV2 SFP RX Issue</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160ARDB-REV2-SFP-RX-Issue/m-p/1404221#M9923</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Please check the attachments.&lt;/P&gt;&lt;P&gt;Including uboot log, serdes1-sch and clockgen-sch.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jan 2022 01:38:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160ARDB-REV2-SFP-RX-Issue/m-p/1404221#M9923</guid>
      <dc:creator>tsungmin_wang</dc:creator>
      <dc:date>2022-01-25T01:38:10Z</dc:date>
    </item>
  </channel>
</rss>