<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: Debug Option</title>
    <link>https://community.nxp.com/t5/Layerscape/Debug-Option/m-p/1403553#M9902</link>
    <description>&lt;P&gt;CMSIS-DAP is a low-speed debugger, accessible from the USB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt; we are planning to go with JTAG instead of CMSIS DAP for programming&lt;/P&gt;&lt;P&gt;&amp;gt; and debugging. Would that be fine?&lt;/P&gt;&lt;P&gt;Yes, it will be.&lt;/P&gt;&lt;P&gt;CMSIS-DAP is an optional module - i.e. JTAG can be used for the board bring-up solely.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt; Also kindly mention the additional changes that would be required if go with the above mentioned design.&lt;/P&gt;&lt;P&gt;Just not implement the CMSIS-DAP module.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt; Also will be compromising on any functionality if we avoid CMSIS DAP?&lt;/P&gt;&lt;P&gt;The whole LS1012A debug functionality is available through JTAG interface.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt; Can you please explain the use case of CMSIS_DAP(MK20DX128VFM5) Interface?&lt;/P&gt;&lt;P&gt;Please refer for example to the QorIQ LS1012A Reference Design Board Manual, 2.18.1 CMSIS-DAP.&lt;/P&gt;</description>
    <pubDate>Sat, 22 Jan 2022 17:29:57 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2022-01-22T17:29:57Z</dc:date>
    <item>
      <title>Debug Option</title>
      <link>https://community.nxp.com/t5/Layerscape/Debug-Option/m-p/1403531#M9900</link>
      <description>&lt;P&gt;Hi NXP Team,&lt;/P&gt;&lt;P&gt;We are planning to develop a custom board based on LS1012A but we have space constraint. So we are planning to go with JTAG instead of CMSIS DAP for programming and debugging. Would that be fine?.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also kindly mention the additional changes that would be required if go with the above mentioned design.&lt;/P&gt;&lt;P&gt;Also will be compromising on any functionality if we avoid CMSIS DAP?&lt;/P&gt;&lt;P&gt;Can you please explain the use case of CMSIS_DAP(MK20DX128VFM5) Interface?&lt;/P&gt;&lt;P&gt;This CMSIS-DAP is used in all reference designs of LS1012A, so please clear this doubt and share interface diagram&lt;/P&gt;</description>
      <pubDate>Sat, 22 Jan 2022 11:38:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Debug-Option/m-p/1403531#M9900</guid>
      <dc:creator>g_reshmi</dc:creator>
      <dc:date>2022-01-22T11:38:41Z</dc:date>
    </item>
    <item>
      <title>Re: Debug Option</title>
      <link>https://community.nxp.com/t5/Layerscape/Debug-Option/m-p/1403553#M9902</link>
      <description>&lt;P&gt;CMSIS-DAP is a low-speed debugger, accessible from the USB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt; we are planning to go with JTAG instead of CMSIS DAP for programming&lt;/P&gt;&lt;P&gt;&amp;gt; and debugging. Would that be fine?&lt;/P&gt;&lt;P&gt;Yes, it will be.&lt;/P&gt;&lt;P&gt;CMSIS-DAP is an optional module - i.e. JTAG can be used for the board bring-up solely.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt; Also kindly mention the additional changes that would be required if go with the above mentioned design.&lt;/P&gt;&lt;P&gt;Just not implement the CMSIS-DAP module.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt; Also will be compromising on any functionality if we avoid CMSIS DAP?&lt;/P&gt;&lt;P&gt;The whole LS1012A debug functionality is available through JTAG interface.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt; Can you please explain the use case of CMSIS_DAP(MK20DX128VFM5) Interface?&lt;/P&gt;&lt;P&gt;Please refer for example to the QorIQ LS1012A Reference Design Board Manual, 2.18.1 CMSIS-DAP.&lt;/P&gt;</description>
      <pubDate>Sat, 22 Jan 2022 17:29:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Debug-Option/m-p/1403553#M9902</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2022-01-22T17:29:57Z</dc:date>
    </item>
  </channel>
</rss>