<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1046A watchdog force pull high/low in u-boot</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046A-watchdog-force-pull-high-low-in-u-boot/m-p/1400557#M9857</link>
    <description>&lt;P&gt;Yes, &lt;SPAN&gt;GPIO2_2/GPIO2_3 pins is already set in RCW.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 18 Jan 2022 02:11:51 GMT</pubDate>
    <dc:creator>charleshuang</dc:creator>
    <dc:date>2022-01-18T02:11:51Z</dc:date>
    <item>
      <title>LS1046A watchdog force pull high/low in u-boot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-watchdog-force-pull-high-low-in-u-boot/m-p/1397231#M9811</link>
      <description>&lt;P&gt;Hi NXP Team.&lt;/P&gt;&lt;P&gt;We want to force pull-high or pull-low the&amp;nbsp;&lt;SPAN&gt;Enable/Trigger pins in U-Boot.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So we add some code as below, but it look like no use.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Do you have any suggestion for us ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Enable pin =&amp;gt; GPIO2_2&lt;/P&gt;&lt;P&gt;Trigger pin =&amp;gt; GPIO2_3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;*** u-boot/board/freescale/ls1046ardb/ls1046ardb.c&amp;nbsp; ***&lt;/P&gt;&lt;P&gt;#define WDT_DIRMASK_TRIG 0xefffffff&lt;BR /&gt;#define WDT_DATMASK_TRIG 0x10000000&lt;BR /&gt;#define WDT_DIRMASK_EN 0xdfffffff&lt;BR /&gt;#define WDT_DATMASK_EN 0xdfffffff&lt;/P&gt;&lt;P&gt;static inline void wdt_pinmux_init(void)&lt;BR /&gt;{&lt;BR /&gt;u32 val;&lt;BR /&gt;struct ccsr_gpio *pgpio = (void *)(GPIO2_BASE_ADDR);&lt;/P&gt;&lt;P&gt;/* en pin */&lt;BR /&gt;val = in_be32(&amp;amp;pgpio-&amp;gt;gpdir);&lt;BR /&gt;val &amp;amp;= WDT_DIRMASK_EN;&lt;BR /&gt;out_be32(&amp;amp;pgpio-&amp;gt;gpdir, val);&lt;/P&gt;&lt;P&gt;printf("WDT_DIRMASK_EN val (0x%X)\n", val);&lt;/P&gt;&lt;P&gt;val = in_be32(&amp;amp;pgpio-&amp;gt;gpdat);&lt;BR /&gt;val &amp;amp;= WDT_DATMASK_EN;&lt;BR /&gt;out_be32(&amp;amp;pgpio-&amp;gt;gpdat, val);&lt;/P&gt;&lt;P&gt;printf("WDT_DATMASK_EN val (0x%X)\n", val);&lt;/P&gt;&lt;P&gt;/* trig pin */&lt;BR /&gt;val = in_be32(&amp;amp;pgpio-&amp;gt;gpdir);&lt;BR /&gt;val &amp;amp;= WDT_DIRMASK_TRIG;&lt;BR /&gt;out_be32(&amp;amp;pgpio-&amp;gt;gpdir, val);&lt;/P&gt;&lt;P&gt;printf("WDT_DIRMASK_TRIG val (0x%X)\n", val);&lt;/P&gt;&lt;P&gt;val = in_be32(&amp;amp;pgpio-&amp;gt;gpdat);&lt;BR /&gt;val |= WDT_DATMASK_TRIG;&lt;BR /&gt;out_be32(&amp;amp;pgpio-&amp;gt;gpdat, val);&lt;/P&gt;&lt;P&gt;printf("WDT_DATMASK_TRIG val (0x%X)\n", val);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;void config_board_mux(void)&lt;BR /&gt;{&lt;/P&gt;&lt;P&gt;.....&lt;/P&gt;&lt;P&gt;/* adv-wdt mux init */&lt;BR /&gt;wdt_pinmux_init();&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jan 2022 08:37:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-watchdog-force-pull-high-low-in-u-boot/m-p/1397231#M9811</guid>
      <dc:creator>charleshuang</dc:creator>
      <dc:date>2022-01-11T08:37:31Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A watchdog force pull high/low in u-boot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-watchdog-force-pull-high-low-in-u-boot/m-p/1399263#M9840</link>
      <description>&lt;P&gt;Are these pins assigned to GPIO in the LS1046a RCW?&lt;/P&gt;
&lt;P&gt;See the Section 3.4.6 in the LS1046a Reference Manual:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=LS1046ARM" target="_blank" rel="noopener"&gt;https://www.nxp.com/webapp/Download?colCode=LS1046ARM&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jan 2022 05:33:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-watchdog-force-pull-high-low-in-u-boot/m-p/1399263#M9840</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2022-01-14T05:33:20Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A watchdog force pull high/low in u-boot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-watchdog-force-pull-high-low-in-u-boot/m-p/1400557#M9857</link>
      <description>&lt;P&gt;Yes, &lt;SPAN&gt;GPIO2_2/GPIO2_3 pins is already set in RCW.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jan 2022 02:11:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-watchdog-force-pull-high-low-in-u-boot/m-p/1400557#M9857</guid>
      <dc:creator>charleshuang</dc:creator>
      <dc:date>2022-01-18T02:11:51Z</dc:date>
    </item>
  </channel>
</rss>