<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: pcie  COMPLIANCE  test</title>
    <link>https://community.nxp.com/t5/Layerscape/pcie-COMPLIANCE-test/m-p/1398657#M9829</link>
    <description>&lt;P&gt;The devices accompanying the signal integrity test do not need to be identified. I can confirm that our hardware design is ok because normal pcie storage devices and network cards can be identified。&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'm now plugging in a storage device，uboot log：&lt;/SPAN&gt;&lt;BR /&gt;PCIe6: pcie@3900000 Root Complex: x4 gen3&lt;/P&gt;&lt;P&gt;=&amp;gt; pci 6&lt;BR /&gt;Scanning PCI devices on bus 6&lt;BR /&gt;BusDevFun VendorId DeviceId Device Class Sub-Class&lt;BR /&gt;_____________________________________________________________&lt;BR /&gt;06.00.00 0x1957 0x8d82 Bridge device 0x04&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 13 Jan 2022 08:11:02 GMT</pubDate>
    <dc:creator>muaxi8</dc:creator>
    <dc:date>2022-01-13T08:11:02Z</dc:date>
    <item>
      <title>pcie  COMPLIANCE  test</title>
      <link>https://community.nxp.com/t5/Layerscape/pcie-COMPLIANCE-test/m-p/1398095#M9819</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Now our LX2180 board needs to perform pcie signal integrity test, but the pcie state machine &lt;FONT color="#FF6600"&gt;cannot&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;FONT color="#FF6600"&gt;enter POLL_COMPLIANCE state&lt;/FONT&gt;, it alaways in the detect_quiet state, and the COMPLIANCE state&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;kernel configuration is only imX.6/7/8&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;Is there a register that can configure the state machine to COMPLIANCE?&lt;/SPAN&gt;&lt;SPAN class=""&gt; Or otherwise configure the&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;COMPLIANCE status?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="muaxi8_0-1641989129434.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/167420i0D12646E97A1179A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="muaxi8_0-1641989129434.png" alt="muaxi8_0-1641989129434.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="muaxi8_0-1641990388627.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/167421iF367A134C0C288AE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="muaxi8_0-1641990388627.png" alt="muaxi8_0-1641990388627.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jan 2022 12:26:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/pcie-COMPLIANCE-test/m-p/1398095#M9819</guid>
      <dc:creator>muaxi8</dc:creator>
      <dc:date>2022-01-12T12:26:48Z</dc:date>
    </item>
    <item>
      <title>Re: pcie  COMPLIANCE  test</title>
      <link>https://community.nxp.com/t5/Layerscape/pcie-COMPLIANCE-test/m-p/1398152#M9821</link>
      <description>&lt;P&gt;For PCIe electrical compliance testing, the PCI-SIG offered two kinds of boards to facilitate the test for different device type/mode - RC in PC MB formfactor or EP in Plug-in Card formfactor: &lt;BR /&gt;· CBB w/Slot is for EP testing&lt;BR /&gt;o The CBB is in MB formfactor with slots so that the DUT EP can be plugged into the CBB slot for testing&lt;BR /&gt;· CLB w/Gold-Finger is for RC testing&lt;BR /&gt;o The CLB is in Plug-in Card formfactor so that it can be plugged into the DUT RC’s slot for testing&lt;/P&gt;
&lt;P&gt;How exactly PCIe is connected in your case?&lt;/P&gt;
&lt;P&gt;Please provide connection block diagram and corresponding U-Boot booting log as text file.&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jan 2022 14:15:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/pcie-COMPLIANCE-test/m-p/1398152#M9821</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2022-01-12T14:15:41Z</dc:date>
    </item>
    <item>
      <title>Re: pcie  COMPLIANCE  test</title>
      <link>https://community.nxp.com/t5/Layerscape/pcie-COMPLIANCE-test/m-p/1398517#M9824</link>
      <description>&lt;P&gt;&lt;SPAN&gt;My question now is the same as this post&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/Layerscape/LS1046A-PCIe-compliance-mode-set-speed-to-5Gbit-s/m-p/809940" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/Layerscape/LS1046A-PCIe-compliance-mode-set-speed-to-5Gbit-s/m-p/809940&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2.5Gbit/s signal we can see that it is the first state of the pcie state machine. Now we want to configure&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;the&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;status of LX2080 for Compliance to test the 5Gbit/s signal.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We are configured this way，But the 5Gbit/s signal is not visible.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;a. Set the Target link speed bit field (T_LS) to the desired speed (0x2). &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;b. Set the Enter Compliance (EC) bit&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="muaxi8_1-1642040626198.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/167477iCDF9A36A0D0B798F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="muaxi8_1-1642040626198.png" alt="muaxi8_1-1642040626198.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jan 2022 02:26:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/pcie-COMPLIANCE-test/m-p/1398517#M9824</guid>
      <dc:creator>muaxi8</dc:creator>
      <dc:date>2022-01-13T02:26:15Z</dc:date>
    </item>
    <item>
      <title>Re: pcie  COMPLIANCE  test</title>
      <link>https://community.nxp.com/t5/Layerscape/pcie-COMPLIANCE-test/m-p/1398607#M9825</link>
      <description>&lt;P&gt;Please provide additional information:&lt;/P&gt;
&lt;P&gt;1) the processor connection schematics as searchable PDF to check PCIe links connections&lt;/P&gt;
&lt;P&gt;2) U-Boot booting log as text file.&lt;/P&gt;
&lt;P&gt;3) which exactly PCIe controller is tested?&lt;/P&gt;
&lt;P&gt;4) You wrote: "We are configured this way" - please provide corresponding log as text file.&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jan 2022 04:57:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/pcie-COMPLIANCE-test/m-p/1398607#M9825</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2022-01-13T04:57:26Z</dc:date>
    </item>
    <item>
      <title>Re: pcie  COMPLIANCE  test</title>
      <link>https://community.nxp.com/t5/Layerscape/pcie-COMPLIANCE-test/m-p/1398635#M9827</link>
      <description>&lt;P&gt;1)&amp;nbsp;&lt;SPAN&gt;The Uboot is attached&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;2)&amp;nbsp;&lt;SPAN&gt;All six pcie controllers need to be tested. The current test is PCI 6.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;root@localhost:~# ./devmem&lt;/P&gt;&lt;P&gt;Usage: ./devmem { address } [ type [ data ] ]&lt;BR /&gt;address : memory address to act upon&lt;BR /&gt;type : access operation type : [b]yte, [h]alfword, [w]ord&lt;BR /&gt;data : data to be written&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;root@localhost:~# ./devmem 0x39000a0 h&lt;BR /&gt;/dev/mem opened.&lt;BR /&gt;Memory mapped at address 0xffffa6910000.&lt;BR /&gt;Value at address 0x39000A0 (0xffffa69100a0):&lt;FONT color="#FF0000"&gt; 0x3&lt;/FONT&gt;&lt;BR /&gt;root@localhost:~#&lt;BR /&gt;root@localhost:~#&lt;BR /&gt;root@localhost:~# ./devmem 0x39000a0 h 0x13&lt;BR /&gt;/dev/mem opened.&lt;BR /&gt;Memory mapped at address 0xffffb22a2000.&lt;BR /&gt;Value at address 0x39000A0 (0xffffb22a20a0): 0x3&lt;BR /&gt;Written 0x13; readback &lt;FONT color="#FF0000"&gt;0x13&lt;/FONT&gt;&lt;BR /&gt;root@localhost:~# ./devmem 0x39000a0 h&lt;BR /&gt;/dev/mem opened.&lt;BR /&gt;Memory mapped at address 0xffff89496000.&lt;BR /&gt;Value at address 0x39000A0 (0xffff894960a0): 0x13&lt;BR /&gt;root@localhost:~#&lt;BR /&gt;root@localhost:~#&lt;BR /&gt;root@localhost:~# ./devmem 0x39C07FC h&lt;BR /&gt;/dev/mem opened.&lt;BR /&gt;Memory mapped at address 0xffff8cbb1000.&lt;BR /&gt;Value at address 0x39C07FC (0xffff8cbb17fc): 0x3&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Compliance has been configured&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jan 2022 06:02:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/pcie-COMPLIANCE-test/m-p/1398635#M9827</guid>
      <dc:creator>muaxi8</dc:creator>
      <dc:date>2022-01-13T06:02:01Z</dc:date>
    </item>
    <item>
      <title>Re: pcie  COMPLIANCE  test</title>
      <link>https://community.nxp.com/t5/Layerscape/pcie-COMPLIANCE-test/m-p/1398647#M9828</link>
      <description>&lt;P&gt;1) the processor connection schematics as searchable PDF to check PCIe links connections&lt;/P&gt;
&lt;P&gt;2) In the provided "uboot-log.txt"&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;PCIe6: pcie@3900000 Root Complex: no link&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;Which CLB is used for the PCIe6?&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jan 2022 06:14:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/pcie-COMPLIANCE-test/m-p/1398647#M9828</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2022-01-13T06:14:12Z</dc:date>
    </item>
    <item>
      <title>Re: pcie  COMPLIANCE  test</title>
      <link>https://community.nxp.com/t5/Layerscape/pcie-COMPLIANCE-test/m-p/1398657#M9829</link>
      <description>&lt;P&gt;The devices accompanying the signal integrity test do not need to be identified. I can confirm that our hardware design is ok because normal pcie storage devices and network cards can be identified。&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'm now plugging in a storage device，uboot log：&lt;/SPAN&gt;&lt;BR /&gt;PCIe6: pcie@3900000 Root Complex: x4 gen3&lt;/P&gt;&lt;P&gt;=&amp;gt; pci 6&lt;BR /&gt;Scanning PCI devices on bus 6&lt;BR /&gt;BusDevFun VendorId DeviceId Device Class Sub-Class&lt;BR /&gt;_____________________________________________________________&lt;BR /&gt;06.00.00 0x1957 0x8d82 Bridge device 0x04&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jan 2022 08:11:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/pcie-COMPLIANCE-test/m-p/1398657#M9829</guid>
      <dc:creator>muaxi8</dc:creator>
      <dc:date>2022-01-13T08:11:02Z</dc:date>
    </item>
    <item>
      <title>Re: pcie  COMPLIANCE  test</title>
      <link>https://community.nxp.com/t5/Layerscape/pcie-COMPLIANCE-test/m-p/1398734#M9830</link>
      <description>&lt;P&gt;From the log:&lt;/P&gt;&lt;P&gt;&amp;gt; &lt;SPAN&gt;Written 0x13; readback &lt;FONT color="#FF0000"&gt;0x13&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;For Gen2 it should be 0x12.&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jan 2022 08:29:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/pcie-COMPLIANCE-test/m-p/1398734#M9830</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2022-01-13T08:29:40Z</dc:date>
    </item>
    <item>
      <title>Re: pcie  COMPLIANCE  test</title>
      <link>https://community.nxp.com/t5/Layerscape/pcie-COMPLIANCE-test/m-p/1398794#M9833</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Yes, I know this, the output information of uboot was yesterday, we just changed the pcie slot, so there is&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;no corresponding&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jan 2022 09:32:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/pcie-COMPLIANCE-test/m-p/1398794#M9833</guid>
      <dc:creator>muaxi8</dc:creator>
      <dc:date>2022-01-13T09:32:09Z</dc:date>
    </item>
  </channel>
</rss>