<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LS1046ARDB pinmux RCW setting in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-pinmux-RCW-setting/m-p/1396037#M9793</link>
    <description>&lt;P&gt;Hi NXP Team.&lt;/P&gt;&lt;P&gt;We have an External WDT device and the Enable/Trigger line connect to GPIO2_2/GPIO2_03&amp;nbsp;respectively.&lt;/P&gt;&lt;P&gt;Can we set pinmux in RCW file ? How to do it ?&lt;/P&gt;</description>
    <pubDate>Fri, 07 Jan 2022 08:17:18 GMT</pubDate>
    <dc:creator>charleshuang</dc:creator>
    <dc:date>2022-01-07T08:17:18Z</dc:date>
    <item>
      <title>LS1046ARDB pinmux RCW setting</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-pinmux-RCW-setting/m-p/1396037#M9793</link>
      <description>&lt;P&gt;Hi NXP Team.&lt;/P&gt;&lt;P&gt;We have an External WDT device and the Enable/Trigger line connect to GPIO2_2/GPIO2_03&amp;nbsp;respectively.&lt;/P&gt;&lt;P&gt;Can we set pinmux in RCW file ? How to do it ?&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jan 2022 08:17:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-pinmux-RCW-setting/m-p/1396037#M9793</guid>
      <dc:creator>charleshuang</dc:creator>
      <dc:date>2022-01-07T08:17:18Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046ARDB pinmux RCW setting</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-pinmux-RCW-setting/m-p/1396092#M9794</link>
      <description>&lt;P&gt;It is needed to add into the ".rcw" file the following line:&lt;/P&gt;
&lt;P&gt;SPI_BASE=2&lt;/P&gt;
&lt;P&gt;Please note that SPI cannot be used in this case because SPI_SCK is available only when RCW[SPI_EXT]=0 and RCW[SPI_BASE]=0.&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jan 2022 10:04:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-pinmux-RCW-setting/m-p/1396092#M9794</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2022-01-07T10:04:57Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046ARDB pinmux RCW setting</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-pinmux-RCW-setting/m-p/1396452#M9800</link>
      <description>&lt;P&gt;OK, thank you, I try it first .&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jan 2022 00:53:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-pinmux-RCW-setting/m-p/1396452#M9800</guid>
      <dc:creator>charleshuang</dc:creator>
      <dc:date>2022-01-10T00:53:49Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046ARDB pinmux RCW setting</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-pinmux-RCW-setting/m-p/1396705#M9805</link>
      <description>&lt;P&gt;Hi NXP Team.&lt;/P&gt;&lt;P&gt;Theree are another question.&lt;/P&gt;&lt;P&gt;We want to force pull-high or pull-low the&amp;nbsp;&lt;SPAN&gt;Enable/Trigger pins in U-Boot.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Do you have any suggestion for us ?&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jan 2022 10:12:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-pinmux-RCW-setting/m-p/1396705#M9805</guid>
      <dc:creator>charleshuang</dc:creator>
      <dc:date>2022-01-10T10:12:16Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046ARDB pinmux RCW setting</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-pinmux-RCW-setting/m-p/1396735#M9808</link>
      <description>&lt;P&gt;&amp;gt;Theree are another question.&lt;/P&gt;
&lt;P&gt;Please create new Community question.&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jan 2022 11:42:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-pinmux-RCW-setting/m-p/1396735#M9808</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2022-01-10T11:42:15Z</dc:date>
    </item>
  </channel>
</rss>