<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscapeのトピック16-bit QSPI chip with LS1046A-based board</title>
    <link>https://community.nxp.com/t5/Layerscape/16-bit-QSPI-chip-with-LS1046A-based-board/m-p/1395754#M9790</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have a 16-bit QSPI chip we are trying to use as the boot device for our LS1046A-based board.&amp;nbsp; We noticed in the LS1046A FRWY initialization PBI commands there is a command that looks like it's setting the QuadSPI_MCR to 64-bit LE (write 0x550000, 0x000f400c).&lt;/P&gt;&lt;P&gt;Questions:&lt;/P&gt;&lt;P&gt;Are we able to use 16-bit QuadSPI on with the LS1046A? It looks like all the NXP designs use 8-bit QSPI, which is probably compatible with switching the endianness like this.&lt;/P&gt;&lt;P&gt;Will a 16-bit QSPI be able to endian swap on the qspi controller?&lt;/P&gt;</description>
    <pubDate>Thu, 06 Jan 2022 19:21:42 GMT</pubDate>
    <dc:creator>JRRandall</dc:creator>
    <dc:date>2022-01-06T19:21:42Z</dc:date>
    <item>
      <title>16-bit QSPI chip with LS1046A-based board</title>
      <link>https://community.nxp.com/t5/Layerscape/16-bit-QSPI-chip-with-LS1046A-based-board/m-p/1395754#M9790</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have a 16-bit QSPI chip we are trying to use as the boot device for our LS1046A-based board.&amp;nbsp; We noticed in the LS1046A FRWY initialization PBI commands there is a command that looks like it's setting the QuadSPI_MCR to 64-bit LE (write 0x550000, 0x000f400c).&lt;/P&gt;&lt;P&gt;Questions:&lt;/P&gt;&lt;P&gt;Are we able to use 16-bit QuadSPI on with the LS1046A? It looks like all the NXP designs use 8-bit QSPI, which is probably compatible with switching the endianness like this.&lt;/P&gt;&lt;P&gt;Will a 16-bit QSPI be able to endian swap on the qspi controller?&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jan 2022 19:21:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/16-bit-QSPI-chip-with-LS1046A-based-board/m-p/1395754#M9790</guid>
      <dc:creator>JRRandall</dc:creator>
      <dc:date>2022-01-06T19:21:42Z</dc:date>
    </item>
    <item>
      <title>Re: 16-bit QSPI chip with LS1046A-based board</title>
      <link>https://community.nxp.com/t5/Layerscape/16-bit-QSPI-chip-with-LS1046A-based-board/m-p/1395923#M9791</link>
      <description>&lt;P&gt;QSPI controller endianness is configured for internal data exchange and is independent of the connected SPI device.&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jan 2022 05:14:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/16-bit-QSPI-chip-with-LS1046A-based-board/m-p/1395923#M9791</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2022-01-07T05:14:02Z</dc:date>
    </item>
  </channel>
</rss>