<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックTrying to read Reset Request Preboot Loader Status Register on LS1046A using CodeWarrior TAP</title>
    <link>https://community.nxp.com/t5/Layerscape/Trying-to-read-Reset-Request-Preboot-Loader-Status-Register-on/m-p/1394947#M9777</link>
    <description>&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We have a custom board based on the LS1046A that needs to boot from QSPI NOR flash. We are having a problem with the RCW that we put into the QSPI flash. Something goes wrong at power on and the board is not booting.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;In order to debug this, there is a&amp;nbsp;Reset Request Preboot Loader Status Register (RSTR QPBLSR) that we would like to use CodeWarrior TAP to connect to the target and read out while in this state.&amp;nbsp; There is a ERR_CODE bitfield in this register that will hopefully give us some breadcrumbs on where to look next, but I'm having trouble figuring out how to read it with TAP.&amp;nbsp; I don't want an initialization script to reset anything on the target.&amp;nbsp; Just connect and read this status register.&amp;nbsp; How can I accomplish this using CodeWarrior TAP?&amp;nbsp; I.e. read&amp;nbsp;CFG_CCSR_RSTRQPBLSR[ERR_CODE].&amp;nbsp; I believe for the LS1046A this would be base address&amp;nbsp;1EE_0084 for error register&lt;/P&gt;</description>
    <pubDate>Wed, 05 Jan 2022 16:30:27 GMT</pubDate>
    <dc:creator>JRRandall</dc:creator>
    <dc:date>2022-01-05T16:30:27Z</dc:date>
    <item>
      <title>Trying to read Reset Request Preboot Loader Status Register on LS1046A using CodeWarrior TAP</title>
      <link>https://community.nxp.com/t5/Layerscape/Trying-to-read-Reset-Request-Preboot-Loader-Status-Register-on/m-p/1394947#M9777</link>
      <description>&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We have a custom board based on the LS1046A that needs to boot from QSPI NOR flash. We are having a problem with the RCW that we put into the QSPI flash. Something goes wrong at power on and the board is not booting.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;In order to debug this, there is a&amp;nbsp;Reset Request Preboot Loader Status Register (RSTR QPBLSR) that we would like to use CodeWarrior TAP to connect to the target and read out while in this state.&amp;nbsp; There is a ERR_CODE bitfield in this register that will hopefully give us some breadcrumbs on where to look next, but I'm having trouble figuring out how to read it with TAP.&amp;nbsp; I don't want an initialization script to reset anything on the target.&amp;nbsp; Just connect and read this status register.&amp;nbsp; How can I accomplish this using CodeWarrior TAP?&amp;nbsp; I.e. read&amp;nbsp;CFG_CCSR_RSTRQPBLSR[ERR_CODE].&amp;nbsp; I believe for the LS1046A this would be base address&amp;nbsp;1EE_0084 for error register&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jan 2022 16:30:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Trying-to-read-Reset-Request-Preboot-Loader-Status-Register-on/m-p/1394947#M9777</guid>
      <dc:creator>JRRandall</dc:creator>
      <dc:date>2022-01-05T16:30:27Z</dc:date>
    </item>
    <item>
      <title>Re: Trying to read Reset Request Preboot Loader Status Register on LS1046A using CodeWarrior TAP</title>
      <link>https://community.nxp.com/t5/Layerscape/Trying-to-read-Reset-Request-Preboot-Loader-Status-Register-on/m-p/1395322#M9782</link>
      <description>&lt;P&gt;Please confirm that RESET_REQ_B assertion does not generate PORESET_B in your case.&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jan 2022 05:15:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Trying-to-read-Reset-Request-Preboot-Loader-Status-Register-on/m-p/1395322#M9782</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2022-01-06T05:15:11Z</dc:date>
    </item>
  </channel>
</rss>