<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is there any simple LS1043A DPAA reference driver other than Linux/U-Boot? in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Is-there-any-simple-LS1043A-DPAA-reference-driver-other-than/m-p/1393583#M9761</link>
    <description>&lt;P&gt;I am developing LS1043A Ethernet driver for a RTOS. I could check the communication on Independent Mode, and I want to add the QMAN and BMAN functionality now.&lt;/P&gt;&lt;P&gt;I referred U-Boot source for Independent Mode settings. But, since U-Boot does not support QMAN and BMAN, I have to refer some other source for these settings.&lt;/P&gt;&lt;P&gt;Is there any simple driver similar to U-Boot which I can refer to QMAN and BMAN initialization and settings? Is there any Application notes which describe more detailed on QMAN and BMAN settings?&lt;/P&gt;&lt;P&gt;Since Linux seems to be complex to me, I want to refer some other simple source. Kindly let me know.&lt;/P&gt;</description>
    <pubDate>Sat, 01 Jan 2022 03:19:15 GMT</pubDate>
    <dc:creator>sempori</dc:creator>
    <dc:date>2022-01-01T03:19:15Z</dc:date>
    <item>
      <title>Is there any simple LS1043A DPAA reference driver other than Linux/U-Boot?</title>
      <link>https://community.nxp.com/t5/Layerscape/Is-there-any-simple-LS1043A-DPAA-reference-driver-other-than/m-p/1393583#M9761</link>
      <description>&lt;P&gt;I am developing LS1043A Ethernet driver for a RTOS. I could check the communication on Independent Mode, and I want to add the QMAN and BMAN functionality now.&lt;/P&gt;&lt;P&gt;I referred U-Boot source for Independent Mode settings. But, since U-Boot does not support QMAN and BMAN, I have to refer some other source for these settings.&lt;/P&gt;&lt;P&gt;Is there any simple driver similar to U-Boot which I can refer to QMAN and BMAN initialization and settings? Is there any Application notes which describe more detailed on QMAN and BMAN settings?&lt;/P&gt;&lt;P&gt;Since Linux seems to be complex to me, I want to refer some other simple source. Kindly let me know.&lt;/P&gt;</description>
      <pubDate>Sat, 01 Jan 2022 03:19:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Is-there-any-simple-LS1043A-DPAA-reference-driver-other-than/m-p/1393583#M9761</guid>
      <dc:creator>sempori</dc:creator>
      <dc:date>2022-01-01T03:19:15Z</dc:date>
    </item>
    <item>
      <title>Re: Is there any simple LS1043A DPAA reference driver other than Linux/U-Boot?</title>
      <link>https://community.nxp.com/t5/Layerscape/Is-there-any-simple-LS1043A-DPAA-reference-driver-other-than/m-p/1393584#M9762</link>
      <description>&lt;P&gt;&amp;gt; Is there any simple driver similar to U-Boot which I can refer to QMAN and BMAN initialization and settings&lt;/P&gt;
&lt;P&gt;There is no such simple driver.&lt;/P&gt;
&lt;P&gt;&amp;gt; Is there any Application notes which describe more detailed on QMAN and BMAN settings?&lt;/P&gt;
&lt;P&gt;QMAN and BMAN are described in the QorIQ LS1043A Data Path Acceleration Architecture (DPAA) Reference Manual.&lt;/P&gt;</description>
      <pubDate>Sat, 01 Jan 2022 06:47:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Is-there-any-simple-LS1043A-DPAA-reference-driver-other-than/m-p/1393584#M9762</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2022-01-01T06:47:40Z</dc:date>
    </item>
    <item>
      <title>Re: Is there any simple LS1043A DPAA reference driver other than Linux/U-Boot?</title>
      <link>https://community.nxp.com/t5/Layerscape/Is-there-any-simple-LS1043A-DPAA-reference-driver-other-than/m-p/1393600#M9763</link>
      <description>&lt;P&gt;If so, Kindly let me know which source files in Linux can I refer for the QMAN, BMAN and FMAN settings for LS1043ARDB board specific?&lt;/P&gt;</description>
      <pubDate>Sun, 02 Jan 2022 01:26:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Is-there-any-simple-LS1043A-DPAA-reference-driver-other-than/m-p/1393600#M9763</guid>
      <dc:creator>sempori</dc:creator>
      <dc:date>2022-01-02T01:26:29Z</dc:date>
    </item>
    <item>
      <title>Re: Is there any simple LS1043A DPAA reference driver other than Linux/U-Boot?</title>
      <link>https://community.nxp.com/t5/Layerscape/Is-there-any-simple-LS1043A-DPAA-reference-driver-other-than/m-p/1393603#M9764</link>
      <description>&lt;P&gt;Please read the Layerscape Software Development Kit User Guide:&lt;/P&gt;&lt;P&gt;&lt;A href="https://docs.nxp.com/bundle/GUID-487B2E69-BB19-42CB-AC38-7EF18C0FE3AE/page/GUID-BC6368BD-C2FB-4284-AD51-AE9F990F1AE5.html" target="_blank"&gt;https://docs.nxp.com/bundle/GUID-487B2E69-BB19-42CB-AC38-7EF18C0FE3AE/page/GUID-BC6368BD-C2FB-4284-AD51-AE9F990F1AE5.html&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 02 Jan 2022 04:44:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Is-there-any-simple-LS1043A-DPAA-reference-driver-other-than/m-p/1393603#M9764</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2022-01-02T04:44:28Z</dc:date>
    </item>
    <item>
      <title>Re: Is there any simple LS1043A DPAA reference driver other than Linux/U-Boot?</title>
      <link>https://community.nxp.com/t5/Layerscape/Is-there-any-simple-LS1043A-DPAA-reference-driver-other-than/m-p/1394795#M9775</link>
      <description>&lt;P&gt;Kindly let me know is there any way to dump the registers values of BMan, QMan and FMan in Linux? I would like to check the register settings with my driver. It is extremely difficult to trace through the Linux code to know about the settings of them. Please help me.&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jan 2022 11:32:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Is-there-any-simple-LS1043A-DPAA-reference-driver-other-than/m-p/1394795#M9775</guid>
      <dc:creator>sempori</dc:creator>
      <dc:date>2022-01-05T11:32:33Z</dc:date>
    </item>
    <item>
      <title>Re: Is there any simple LS1043A DPAA reference driver other than Linux/U-Boot?</title>
      <link>https://community.nxp.com/t5/Layerscape/Is-there-any-simple-LS1043A-DPAA-reference-driver-other-than/m-p/1394814#M9776</link>
      <description>&lt;P&gt;There is no off-the-shelf tool to perform requested registers dumps.&lt;/P&gt;
&lt;P&gt;You either have to implement it yourself or apply to the paid NXP Engineering Services:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/support/support/nxp-engineering-services:SW-SUPPORT" target="_blank"&gt;https://www.nxp.com/support/support/nxp-engineering-services:SW-SUPPORT&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jan 2022 12:14:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Is-there-any-simple-LS1043A-DPAA-reference-driver-other-than/m-p/1394814#M9776</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2022-01-05T12:14:39Z</dc:date>
    </item>
  </channel>
</rss>