<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1012A Serdes options</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1012A-Serdes-options/m-p/1393269#M9752</link>
    <description>&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;If the 100Mhz reference clock provided by a PCIe RC is not a spread-spectrum，SGMII can work,right?&lt;/P&gt;</description>
    <pubDate>Thu, 30 Dec 2021 07:36:40 GMT</pubDate>
    <dc:creator>victor0123</dc:creator>
    <dc:date>2021-12-30T07:36:40Z</dc:date>
    <item>
      <title>LS1012A Serdes options</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-Serdes-options/m-p/1393190#M9750</link>
      <description>&lt;P&gt;In my PCB,LS1012A Serdes lane A:SGMII1,lane B:SGMII2,lane D:PCIE(Endpoint).&lt;/P&gt;&lt;P&gt;SRDS_PRTCL_S1 RCW[128:143]=3305.&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;SD1_REF_CLK1_P/&lt;/SPAN&gt;N PIN is &lt;SPAN class=""&gt;provided&lt;/SPAN&gt; 100Mhz from X86 DEMO.&lt;/P&gt;&lt;P&gt;The PCIE of X86 DEMO is &lt;SPAN class=""&gt;configured to operate as a PCI Express Root Complex.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;LS1012A is configured to operate as a Endpoint device.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;But &amp;lt;QorIQ LS1012A Reference Manual&amp;nbsp; &amp;gt;Page 234&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="victor0123_0-1640835261838.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/166479iE8471520DC1525AF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="victor0123_0-1640835261838.png" alt="victor0123_0-1640835261838.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;victor0123_0-1640835261838.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Setting this bit to 0 is only supported with&lt;BR /&gt;SerDes protocol option (SRDS_PRTCL_S1) =&lt;BR /&gt;0x0005 ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;SGMII1 and SGMII2 can not work?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 30 Dec 2021 05:30:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-Serdes-options/m-p/1393190#M9750</guid>
      <dc:creator>victor0123</dc:creator>
      <dc:date>2021-12-30T05:30:24Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012A Serdes options</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-Serdes-options/m-p/1393220#M9751</link>
      <description>&lt;P&gt;Proper operation of &lt;SPAN class=""&gt;SGMII1 and SGMII2&lt;/SPAN&gt; cannot be guaranteed when LS1012A SerDes reference clock is provided by a PCIe RC because spread-spectrum can be used.&lt;/P&gt;</description>
      <pubDate>Thu, 30 Dec 2021 05:52:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-Serdes-options/m-p/1393220#M9751</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-12-30T05:52:17Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012A Serdes options</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-Serdes-options/m-p/1393269#M9752</link>
      <description>&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;If the 100Mhz reference clock provided by a PCIe RC is not a spread-spectrum，SGMII can work,right?&lt;/P&gt;</description>
      <pubDate>Thu, 30 Dec 2021 07:36:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-Serdes-options/m-p/1393269#M9752</guid>
      <dc:creator>victor0123</dc:creator>
      <dc:date>2021-12-30T07:36:40Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012A Serdes options</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-Serdes-options/m-p/1393281#M9753</link>
      <description>&lt;P&gt;Technically SGMII should work in the described case, but configuration in question was not validated during LS1012A silicon bring-up.&lt;/P&gt;</description>
      <pubDate>Thu, 30 Dec 2021 08:01:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-Serdes-options/m-p/1393281#M9753</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-12-30T08:01:03Z</dc:date>
    </item>
  </channel>
</rss>