<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: LS1046 PTP EXTTS configuration.</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046-PTP-EXTTS-configuration/m-p/1385636#M9638</link>
    <description>&lt;P&gt;According to the LS1046A datasheet this pin buffer powered by LVDD and LVDD can be 1.8V or 2.5V. LVDD based receivers are simple CMOS I/O circuits and satisfy appropriate LVCMOS type specifications. The datasheet Table 3 “Absolute maximum ratings for input signal voltage levels” says that Max DC V input range is GND to (LVDD x 1.1). The datasheet section “IEEE 1588 DC electrical characteristics” provides the VIH/VIL (Input high/low voltage).&lt;/P&gt;
&lt;P&gt;The internal pull-up resistor cannot be enabled after PORESET is negation.&lt;/P&gt;</description>
    <pubDate>Mon, 13 Dec 2021 11:56:36 GMT</pubDate>
    <dc:creator>r8070z</dc:creator>
    <dc:date>2021-12-13T11:56:36Z</dc:date>
    <item>
      <title>LS1046 PTP EXTTS configuration.</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-PTP-EXTTS-configuration/m-p/1384760#M9629</link>
      <description>&lt;P&gt;I am going to use External Time Stamps for PTP timer on LS1046A CPU. Now I need to configure an input pin to be used as a&amp;nbsp;TSEC1588_TRIG_IN1. According to "LS1046A Reference Manual" I need to modify the &lt;STRONG&gt;RCW[EC2] = 010&lt;/STRONG&gt;. So I introduced the following change to my 'rcw' source file:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;...
#include &amp;lt;ls1046a.rcwi&amp;gt;                                                 
+ EC2=2
...&lt;/LI-CODE&gt;&lt;P&gt;Beforehand these pins controlled by&amp;nbsp;&lt;STRONG&gt;RCW[EC2]&lt;/STRONG&gt;&amp;nbsp;(EC2_RX_DV, EC2_RXD[0], EC2_RXD[1], etc )were used to communicate with RGMII PHY and the voltage they used was 1.8v.&lt;/P&gt;&lt;P&gt;What voltage (3.3v or 1.8v) can I apply to&amp;nbsp;TSEC1588_TRIG_IN1 pin after setting&amp;nbsp;&lt;STRONG&gt;RCW[EC2] &lt;/STRONG&gt;to '010' ?&lt;/P&gt;&lt;P&gt;Can I enable the internal pull-up resistor somehow on TSEC1588_TRIG_IN1 pin?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 10 Dec 2021 09:39:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-PTP-EXTTS-configuration/m-p/1384760#M9629</guid>
      <dc:creator>Oleksandr1</dc:creator>
      <dc:date>2021-12-10T09:39:56Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046 PTP EXTTS configuration.</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-PTP-EXTTS-configuration/m-p/1385636#M9638</link>
      <description>&lt;P&gt;According to the LS1046A datasheet this pin buffer powered by LVDD and LVDD can be 1.8V or 2.5V. LVDD based receivers are simple CMOS I/O circuits and satisfy appropriate LVCMOS type specifications. The datasheet Table 3 “Absolute maximum ratings for input signal voltage levels” says that Max DC V input range is GND to (LVDD x 1.1). The datasheet section “IEEE 1588 DC electrical characteristics” provides the VIH/VIL (Input high/low voltage).&lt;/P&gt;
&lt;P&gt;The internal pull-up resistor cannot be enabled after PORESET is negation.&lt;/P&gt;</description>
      <pubDate>Mon, 13 Dec 2021 11:56:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-PTP-EXTTS-configuration/m-p/1385636#M9638</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2021-12-13T11:56:36Z</dc:date>
    </item>
  </channel>
</rss>