<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscapeのトピックls1028 can't reboot</title>
    <link>https://community.nxp.com/t5/Layerscape/ls1028-can-t-reboot/m-p/1384700#M9628</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We have a ls1028 customer&amp;nbsp; board, build the system with OpenIL V1.10 ,used the configs&amp;nbsp;nxp_ls1028ardb-64b_defconfig.&amp;nbsp;&lt;/SPAN&gt;When reboot the system, the print log is normal, but the system is stuck at the end of the exiting.&lt;/P&gt;&lt;P&gt;[root@LS1028ARDB ~] # reboot&lt;/P&gt;&lt;P&gt;Stopping Netopeer2-server: OK&lt;BR /&gt;- SSH hostkey found, no need to generate a new one.&lt;BR /&gt;Stopping rootfs-resize: OK&lt;BR /&gt;Stopping sysrepo-tsn: OK&lt;BR /&gt;Stopping sysrepo-plugind: OK&lt;BR /&gt;Stopping sysrepod: OK&lt;BR /&gt;Stopping sshd: OK&lt;BR /&gt;Stopping dhcpcd...&lt;BR /&gt;stopped /sbin/dhcpcd (pid 361)&lt;BR /&gt;Stopping network: OK&lt;BR /&gt;Stopping system message bus: done&lt;BR /&gt;Stopping haveged: stopped /usr/sbin/haveged (pid 294)&lt;BR /&gt;OK&lt;BR /&gt;Saving random seed: OK&lt;BR /&gt;Stopping klogd: OK&lt;BR /&gt;Stopping syslogd: OK&lt;BR /&gt;umount: devtmpfs busy - remounted read-only&lt;BR /&gt;[ 20.905084] 001: EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)&lt;BR /&gt;The system is going down NOW!&lt;BR /&gt;Sent SIGTERM to all processes&lt;BR /&gt;logout&lt;BR /&gt;Sent SIGKILL to all processes&lt;BR /&gt;Requesting system reboot&lt;BR /&gt;[ 22.912562] 000: kvm: exiting hardware virtualization&lt;/P&gt;</description>
    <pubDate>Fri, 10 Dec 2021 08:34:09 GMT</pubDate>
    <dc:creator>Gnimis</dc:creator>
    <dc:date>2021-12-10T08:34:09Z</dc:date>
    <item>
      <title>ls1028 can't reboot</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1028-can-t-reboot/m-p/1384700#M9628</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We have a ls1028 customer&amp;nbsp; board, build the system with OpenIL V1.10 ,used the configs&amp;nbsp;nxp_ls1028ardb-64b_defconfig.&amp;nbsp;&lt;/SPAN&gt;When reboot the system, the print log is normal, but the system is stuck at the end of the exiting.&lt;/P&gt;&lt;P&gt;[root@LS1028ARDB ~] # reboot&lt;/P&gt;&lt;P&gt;Stopping Netopeer2-server: OK&lt;BR /&gt;- SSH hostkey found, no need to generate a new one.&lt;BR /&gt;Stopping rootfs-resize: OK&lt;BR /&gt;Stopping sysrepo-tsn: OK&lt;BR /&gt;Stopping sysrepo-plugind: OK&lt;BR /&gt;Stopping sysrepod: OK&lt;BR /&gt;Stopping sshd: OK&lt;BR /&gt;Stopping dhcpcd...&lt;BR /&gt;stopped /sbin/dhcpcd (pid 361)&lt;BR /&gt;Stopping network: OK&lt;BR /&gt;Stopping system message bus: done&lt;BR /&gt;Stopping haveged: stopped /usr/sbin/haveged (pid 294)&lt;BR /&gt;OK&lt;BR /&gt;Saving random seed: OK&lt;BR /&gt;Stopping klogd: OK&lt;BR /&gt;Stopping syslogd: OK&lt;BR /&gt;umount: devtmpfs busy - remounted read-only&lt;BR /&gt;[ 20.905084] 001: EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)&lt;BR /&gt;The system is going down NOW!&lt;BR /&gt;Sent SIGTERM to all processes&lt;BR /&gt;logout&lt;BR /&gt;Sent SIGKILL to all processes&lt;BR /&gt;Requesting system reboot&lt;BR /&gt;[ 22.912562] 000: kvm: exiting hardware virtualization&lt;/P&gt;</description>
      <pubDate>Fri, 10 Dec 2021 08:34:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1028-can-t-reboot/m-p/1384700#M9628</guid>
      <dc:creator>Gnimis</dc:creator>
      <dc:date>2021-12-10T08:34:09Z</dc:date>
    </item>
    <item>
      <title>Re: ls1028 can't reboot</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1028-can-t-reboot/m-p/1387156#M9651</link>
      <description>&lt;P&gt;I confirmed with the testing team, they didn't encounter reboot problem on ls1028ardb in&amp;nbsp;&lt;SPAN&gt;OpenIL V1.10 testing.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Please check whether this problem is caused by your hardware, please check whether "reset" command can be executed successfully under u-boot.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Dec 2021 08:53:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1028-can-t-reboot/m-p/1387156#M9651</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-12-15T08:53:01Z</dc:date>
    </item>
  </channel>
</rss>