<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: LS1023/LS1043/LS1012A 100BASE-FX support</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1023-LS1043-LS1012A-100BASE-FX-support/m-p/1367407#M9267</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;No, we have on the FPGA side, 100BASE-FX.&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
    <pubDate>Fri, 05 Nov 2021 15:37:33 GMT</pubDate>
    <dc:creator>carlos-m-ribeiro</dc:creator>
    <dc:date>2021-11-05T15:37:33Z</dc:date>
    <item>
      <title>LS1023/LS1043/LS1012A 100BASE-FX support</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1023-LS1043-LS1012A-100BASE-FX-support/m-p/1365700#M9242</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;By default, is there support in u-boot of LS1023/LS1043/LS1012A to connecting directly an 100BASE-FX FPGA to SGMII of LS1023/LS1043/LS1012A?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Nov 2021 10:20:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1023-LS1043-LS1012A-100BASE-FX-support/m-p/1365700#M9242</guid>
      <dc:creator>carlos-m-ribeiro</dc:creator>
      <dc:date>2021-11-03T10:20:12Z</dc:date>
    </item>
    <item>
      <title>Re: LS1023/LS1043/LS1012A 100BASE-FX support</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1023-LS1043-LS1012A-100BASE-FX-support/m-p/1367005#M9256</link>
      <description>&lt;UL&gt;
&lt;LI&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NXP designs to an attachment unit interface (AUI) specification (MII, GMII, RGMII, SGMII, etc.), so in most cases proper operation is achieved if the interface signal requirements (timings, IO levels, etc.) are met. &lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;This includes PHYless designs as well.&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Input Output Buffer Information Specification (IBIS) modeling can help determine signal degradation to/from our device across the interconnect.&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Actual medium support (copper, fiber, coax, etc) is dependent on the Medium Attachment Unit (MAU) connected to our device (PHY, Switch, FPGA, etc). &lt;/SPAN&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;So, 100BASE-FX is not an interface supported by our SoCs.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;SGMII with 8b/10b encoding is the best we have to offer to get 100Mbps with an optical connection.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Can the FPGA connect to the LS device via SGMII?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;As a side note, naming conventions can get confusing. We do list a 1000BASE-X mode but this is really just SGMII with the rate-adaptation logic disabled.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Nov 2021 02:07:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1023-LS1043-LS1012A-100BASE-FX-support/m-p/1367005#M9256</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-11-05T02:07:22Z</dc:date>
    </item>
    <item>
      <title>Re: LS1023/LS1043/LS1012A 100BASE-FX support</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1023-LS1043-LS1012A-100BASE-FX-support/m-p/1367407#M9267</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;No, we have on the FPGA side, 100BASE-FX.&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Fri, 05 Nov 2021 15:37:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1023-LS1043-LS1012A-100BASE-FX-support/m-p/1367407#M9267</guid>
      <dc:creator>carlos-m-ribeiro</dc:creator>
      <dc:date>2021-11-05T15:37:33Z</dc:date>
    </item>
    <item>
      <title>Re: LS1023/LS1043/LS1012A 100BASE-FX support</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1023-LS1043-LS1012A-100BASE-FX-support/m-p/1368167#M9285</link>
      <description>&lt;P&gt;&lt;SPAN&gt;From the AE team.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I tried to put in a slide deck to summarize the supported interfaces by the various controllers. The FPGA must connect to the MAC via a supported interface.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The slide deck is a work in progress. So, please share any corrections or suggestions.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Nov 2021 03:22:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1023-LS1043-LS1012A-100BASE-FX-support/m-p/1368167#M9285</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-11-09T03:22:35Z</dc:date>
    </item>
  </channel>
</rss>