<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: Schematic &amp;amp; Reference manual mismatch</title>
    <link>https://community.nxp.com/t5/Layerscape/Schematic-amp-Reference-manual-mismatch/m-p/1365661#M9241</link>
    <description>&lt;P&gt;“001 {QSPI_A_DATA[3], Reserved, Reserved} NOTE: Must be pulled low when IFC_GRP_A_EXT is selected as 001“ means that when IFC_GRP_A_EXT is selected as 001 there are 2 reserved pins which must be pulled low.&lt;/P&gt;
&lt;P&gt;Attached schematics looks like LS1046ARDB which was designed using preliminary documentation Due to that it shows these 2 pins as QSPI_A_DQS and QSPI_B_DQS. We should follow to the manual recommendation.&lt;/P&gt;</description>
    <pubDate>Wed, 03 Nov 2021 09:36:03 GMT</pubDate>
    <dc:creator>r8070z</dc:creator>
    <dc:date>2021-11-03T09:36:03Z</dc:date>
    <item>
      <title>Schematic &amp; Reference manual mismatch</title>
      <link>https://community.nxp.com/t5/Layerscape/Schematic-amp-Reference-manual-mismatch/m-p/1365172#M9234</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;In LS1046A reference manual, it is mentioned that, QSPI_A_DATA[3] pin should be pulled low when IFC_GRP_A_EXT is selected as 001 (i.e., when pin is used as QSPI_A_DATA[3]). But in the schematics provided, it is not pulled low.&amp;nbsp; Please check and confirm if pull down is required or not.&lt;/P&gt;&lt;P&gt;Attached images (text is highlighted) for your reference.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Tue, 02 Nov 2021 12:44:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Schematic-amp-Reference-manual-mismatch/m-p/1365172#M9234</guid>
      <dc:creator>TrinathK</dc:creator>
      <dc:date>2021-11-02T12:44:29Z</dc:date>
    </item>
    <item>
      <title>Re: Schematic &amp; Reference manual mismatch</title>
      <link>https://community.nxp.com/t5/Layerscape/Schematic-amp-Reference-manual-mismatch/m-p/1365661#M9241</link>
      <description>&lt;P&gt;“001 {QSPI_A_DATA[3], Reserved, Reserved} NOTE: Must be pulled low when IFC_GRP_A_EXT is selected as 001“ means that when IFC_GRP_A_EXT is selected as 001 there are 2 reserved pins which must be pulled low.&lt;/P&gt;
&lt;P&gt;Attached schematics looks like LS1046ARDB which was designed using preliminary documentation Due to that it shows these 2 pins as QSPI_A_DQS and QSPI_B_DQS. We should follow to the manual recommendation.&lt;/P&gt;</description>
      <pubDate>Wed, 03 Nov 2021 09:36:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Schematic-amp-Reference-manual-mismatch/m-p/1365661#M9241</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2021-11-03T09:36:03Z</dc:date>
    </item>
    <item>
      <title>Re: Schematic &amp; Reference manual mismatch</title>
      <link>https://community.nxp.com/t5/Layerscape/Schematic-amp-Reference-manual-mismatch/m-p/1365723#M9243</link>
      <description>&lt;P&gt;Hi Serguei,&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;So you are saying, pull down is applicable only for reserved pins and not for QSPI_A_DATA[3]. But the NOTE mentioned in the reference manual, looks like it is applicable for all the pins mentioned (i.e., QSPI_A_DATA[3], Reserved, Reserved). Please confirm if pull down is required for QSPI_A_DATA[3] or not.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Wed, 03 Nov 2021 11:18:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Schematic-amp-Reference-manual-mismatch/m-p/1365723#M9243</guid>
      <dc:creator>TrinathK</dc:creator>
      <dc:date>2021-11-03T11:18:58Z</dc:date>
    </item>
    <item>
      <title>Re: Schematic &amp; Reference manual mismatch</title>
      <link>https://community.nxp.com/t5/Layerscape/Schematic-amp-Reference-manual-mismatch/m-p/1367158#M9260</link>
      <description>&lt;P&gt;Please see also Table 25. QSPI pin termination checklist in the QorIQ LS1046A Design Checklist , Rev. 2, 06/2020. Pull down for QSPI_A_DATA[3] is not required.&lt;/P&gt;</description>
      <pubDate>Fri, 05 Nov 2021 07:30:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Schematic-amp-Reference-manual-mismatch/m-p/1367158#M9260</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2021-11-05T07:30:58Z</dc:date>
    </item>
  </channel>
</rss>