<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic uboot cause single PFE ethernet ping cmd fail in kernel in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/uboot-cause-single-PFE-ethernet-ping-cmd-fail-in-kernel/m-p/1362986#M9202</link>
    <description>&lt;P&gt;I have a&amp;nbsp; LS1012A rdb alike board from forlinx, , it have two AR8031, one for RGMIII and another for SGMII interface, I add switch button to SGMII AR8031 reset pin, so i can control it work or not, then i change pfe_eth.c and fsl-ls2012a-rdb.dts accroding to&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/Layerscape-Knowledge-Base/Packet-Forwarding-Engine-PFE-Ethernet-Ports-Setting-up-on/ta-p/1114831" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/Layerscape-Knowledge-Base/Packet-Forwarding-Engine-PFE-Ethernet-Ports-Setting-up-on/ta-p/1114831&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;I reset SGMII AR8031 by switch button&amp;nbsp; and boot up system with two ethernet interface,&lt;BR /&gt;&lt;BR /&gt;root@OpenWrt:/# ifconfig&lt;BR /&gt;br-lan Link encap:Ethernet HWaddr 76:0C:45:6A:F6:95&lt;BR /&gt;inet addr:192.168.1.1 Bcast:192.168.1.255 Mask:255.255.255.0&lt;BR /&gt;inet6 addr: fd7f:8300:7042::1/60 Scope:Global&lt;BR /&gt;inet6 addr: fe80::740c:45ff:fe6a:f695/64 Scope:Link&lt;BR /&gt;UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:39 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:4801 (4.6 KiB)&lt;BR /&gt;&lt;BR /&gt;eth0 Link encap:Ethernet HWaddr 76:0C:45:6A:F6:95&lt;BR /&gt;UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:39 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:4801 (4.6 KiB)&lt;BR /&gt;&lt;BR /&gt;eth1 Link encap:Ethernet HWaddr 62:71:65:C8:FA:CE&lt;BR /&gt;inet addr:192.168.3.99 Bcast:192.168.3.255 Mask:255.255.255.0&lt;BR /&gt;inet6 addr: fe80::6071:65ff:fec8:face/64 Scope:Link&lt;BR /&gt;UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:42 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:93 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:56025 (54.7 KiB) TX bytes:23426 (22.8 KiB)&lt;BR /&gt;&lt;BR /&gt;after setup its ip addr, it fail to ping&amp;nbsp; the gateway&lt;BR /&gt;&lt;BR /&gt;root@OpenWrt:/# ifconfig eth1 192.168.3.119&lt;BR /&gt;root@OpenWrt:/# ping 192.168.3.1&lt;BR /&gt;PING 192.168.3.1 (192.168.3.1): 56 data bytes&lt;BR /&gt;&lt;BR /&gt;not response from gateway&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;we fint the the cause related to uboot, it come from forlinx without source code, it only support two ethernet, so uboot will fail to support single FPE ethernet port,&lt;BR /&gt;&lt;BR /&gt;SCSI: Net: PFE class pe firmware&lt;BR /&gt;PFE tmu pe firmware&lt;BR /&gt;pfe_configure_serdes 0&lt;BR /&gt;Could not get PHY for PFE_MDIO: addr 1&lt;BR /&gt;phy_connect failed&lt;BR /&gt;No ethernet found.&lt;BR /&gt;&lt;BR /&gt;but if we let uboot work without reset SGMII AR8031, so it will boot successfully with two ethernet port successfully&lt;BR /&gt;&lt;BR /&gt;SCSI: Net: PFE class pe firmware&lt;BR /&gt;PFE tmu pe firmware&lt;BR /&gt;pfe_configure_serdes 0&lt;BR /&gt;eth0: pfe_eth0, eth1: pfe_eth1&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;=&amp;gt;&lt;BR /&gt;&lt;BR /&gt;the i reset SGMII AR8031 to let openwrt work with&lt;BR /&gt;&lt;BR /&gt;single PFE ethernet port condition&lt;BR /&gt;&lt;BR /&gt;=&amp;gt; pfe stop&lt;BR /&gt;Stopping PFE...&lt;BR /&gt;&lt;BR /&gt;=&amp;gt; ...&lt;BR /&gt;&lt;BR /&gt;and continue boot openwrt system, now the network now work correctly&lt;BR /&gt;&lt;BR /&gt;root@OpenWrt:/# ifconfig eth1 192.168.3.119&lt;BR /&gt;root@OpenWrt:/# ping 192.168.3.1&lt;BR /&gt;PING 192.168.3.1 (192.168.3.1): 56 data bytes&lt;BR /&gt;64 bytes from 192.168.3.1: seq=0 ttl=64 time=8.740 ms&lt;BR /&gt;64 bytes from 192.168.3.1: seq=1 ttl=64 time=1.730 ms&lt;BR /&gt;64 bytes from 192.168.3.1: seq=2 ttl=64 time=2.287 ms&lt;BR /&gt;&lt;BR /&gt;so what can we do to fix this issue? any suggestion is welcome, thanks&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 28 Oct 2021 07:21:33 GMT</pubDate>
    <dc:creator>zhongtao1701</dc:creator>
    <dc:date>2021-10-28T07:21:33Z</dc:date>
    <item>
      <title>uboot cause single PFE ethernet ping cmd fail in kernel</title>
      <link>https://community.nxp.com/t5/Layerscape/uboot-cause-single-PFE-ethernet-ping-cmd-fail-in-kernel/m-p/1362986#M9202</link>
      <description>&lt;P&gt;I have a&amp;nbsp; LS1012A rdb alike board from forlinx, , it have two AR8031, one for RGMIII and another for SGMII interface, I add switch button to SGMII AR8031 reset pin, so i can control it work or not, then i change pfe_eth.c and fsl-ls2012a-rdb.dts accroding to&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/Layerscape-Knowledge-Base/Packet-Forwarding-Engine-PFE-Ethernet-Ports-Setting-up-on/ta-p/1114831" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/Layerscape-Knowledge-Base/Packet-Forwarding-Engine-PFE-Ethernet-Ports-Setting-up-on/ta-p/1114831&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;I reset SGMII AR8031 by switch button&amp;nbsp; and boot up system with two ethernet interface,&lt;BR /&gt;&lt;BR /&gt;root@OpenWrt:/# ifconfig&lt;BR /&gt;br-lan Link encap:Ethernet HWaddr 76:0C:45:6A:F6:95&lt;BR /&gt;inet addr:192.168.1.1 Bcast:192.168.1.255 Mask:255.255.255.0&lt;BR /&gt;inet6 addr: fd7f:8300:7042::1/60 Scope:Global&lt;BR /&gt;inet6 addr: fe80::740c:45ff:fe6a:f695/64 Scope:Link&lt;BR /&gt;UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:39 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:4801 (4.6 KiB)&lt;BR /&gt;&lt;BR /&gt;eth0 Link encap:Ethernet HWaddr 76:0C:45:6A:F6:95&lt;BR /&gt;UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:39 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:4801 (4.6 KiB)&lt;BR /&gt;&lt;BR /&gt;eth1 Link encap:Ethernet HWaddr 62:71:65:C8:FA:CE&lt;BR /&gt;inet addr:192.168.3.99 Bcast:192.168.3.255 Mask:255.255.255.0&lt;BR /&gt;inet6 addr: fe80::6071:65ff:fec8:face/64 Scope:Link&lt;BR /&gt;UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:42 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:93 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:56025 (54.7 KiB) TX bytes:23426 (22.8 KiB)&lt;BR /&gt;&lt;BR /&gt;after setup its ip addr, it fail to ping&amp;nbsp; the gateway&lt;BR /&gt;&lt;BR /&gt;root@OpenWrt:/# ifconfig eth1 192.168.3.119&lt;BR /&gt;root@OpenWrt:/# ping 192.168.3.1&lt;BR /&gt;PING 192.168.3.1 (192.168.3.1): 56 data bytes&lt;BR /&gt;&lt;BR /&gt;not response from gateway&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;we fint the the cause related to uboot, it come from forlinx without source code, it only support two ethernet, so uboot will fail to support single FPE ethernet port,&lt;BR /&gt;&lt;BR /&gt;SCSI: Net: PFE class pe firmware&lt;BR /&gt;PFE tmu pe firmware&lt;BR /&gt;pfe_configure_serdes 0&lt;BR /&gt;Could not get PHY for PFE_MDIO: addr 1&lt;BR /&gt;phy_connect failed&lt;BR /&gt;No ethernet found.&lt;BR /&gt;&lt;BR /&gt;but if we let uboot work without reset SGMII AR8031, so it will boot successfully with two ethernet port successfully&lt;BR /&gt;&lt;BR /&gt;SCSI: Net: PFE class pe firmware&lt;BR /&gt;PFE tmu pe firmware&lt;BR /&gt;pfe_configure_serdes 0&lt;BR /&gt;eth0: pfe_eth0, eth1: pfe_eth1&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;=&amp;gt;&lt;BR /&gt;&lt;BR /&gt;the i reset SGMII AR8031 to let openwrt work with&lt;BR /&gt;&lt;BR /&gt;single PFE ethernet port condition&lt;BR /&gt;&lt;BR /&gt;=&amp;gt; pfe stop&lt;BR /&gt;Stopping PFE...&lt;BR /&gt;&lt;BR /&gt;=&amp;gt; ...&lt;BR /&gt;&lt;BR /&gt;and continue boot openwrt system, now the network now work correctly&lt;BR /&gt;&lt;BR /&gt;root@OpenWrt:/# ifconfig eth1 192.168.3.119&lt;BR /&gt;root@OpenWrt:/# ping 192.168.3.1&lt;BR /&gt;PING 192.168.3.1 (192.168.3.1): 56 data bytes&lt;BR /&gt;64 bytes from 192.168.3.1: seq=0 ttl=64 time=8.740 ms&lt;BR /&gt;64 bytes from 192.168.3.1: seq=1 ttl=64 time=1.730 ms&lt;BR /&gt;64 bytes from 192.168.3.1: seq=2 ttl=64 time=2.287 ms&lt;BR /&gt;&lt;BR /&gt;so what can we do to fix this issue? any suggestion is welcome, thanks&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 28 Oct 2021 07:21:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/uboot-cause-single-PFE-ethernet-ping-cmd-fail-in-kernel/m-p/1362986#M9202</guid>
      <dc:creator>zhongtao1701</dc:creator>
      <dc:date>2021-10-28T07:21:33Z</dc:date>
    </item>
    <item>
      <title>Re: uboot cause single PFE ethernet fail in kernel</title>
      <link>https://community.nxp.com/t5/Layerscape/uboot-cause-single-PFE-ethernet-ping-cmd-fail-in-kernel/m-p/1363047#M9203</link>
      <description>&lt;P&gt;You could download LSDK 20.04&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;In u-boot source code, please modify board/freescale/ls1012ardb/eth.c as the following.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;In LSDK environment, u-boot source code is in packages/firmware/u-boot.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; switch (srds_s1) {&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; case 0x3508:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (!priv-&amp;gt;gemac_port) {&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* MAC1 */&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pfe_set_phy_address_mode(priv-&amp;gt;gemac_port,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CONFIG_PFE_EMAC1_PHY_ADDR,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PHY_INTERFACE_MODE_SGMII);&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; } else {&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;/* MAC2 */&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pfe_set_phy_address_mode(priv-&amp;gt;gemac_port,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CONFIG_PFE_EMAC2_PHY_ADDR,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PHY_INTERFACE_MODE_RGMII_ID);&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; break;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Then in LSDK build environment rebuild u-boot to generate ATF(firmware) image.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;$ rm -rf build/firmware/u-boot/&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;$ flex-builder -c atf -m ls1012ardb -b qspi &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;$ flex-builder -i mkfw -m ls1012ardb -b qspi&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You will get the following result in u-boot.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;=&amp;gt; mdio list&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;PFE_MDIO:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;1 - RealTek RTL8211F &amp;lt;--&amp;gt; pfe_eth1&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;=&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;In recent released LSDK or OpenWrt, if you want to use only RGMII IF with PFE Ethernet &lt;/SPAN&gt;&lt;SPAN&gt;port, you just need to remove "pfe_mac0"(SGMII) definition in the&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;dts file.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 28 Oct 2021 07:23:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/uboot-cause-single-PFE-ethernet-ping-cmd-fail-in-kernel/m-p/1363047#M9203</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-10-28T07:23:42Z</dc:date>
    </item>
    <item>
      <title>Re: uboot cause single PFE ethernet ping cmd fail in kernel</title>
      <link>https://community.nxp.com/t5/Layerscape/uboot-cause-single-PFE-ethernet-ping-cmd-fail-in-kernel/m-p/1363070#M9205</link>
      <description>&lt;P&gt;thanks for your so quick answer, its very helpful, i will contract forlinx to change it and verify it, thanks again&lt;/P&gt;</description>
      <pubDate>Thu, 28 Oct 2021 07:48:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/uboot-cause-single-PFE-ethernet-ping-cmd-fail-in-kernel/m-p/1363070#M9205</guid>
      <dc:creator>zhongtao1701</dc:creator>
      <dc:date>2021-10-28T07:48:17Z</dc:date>
    </item>
  </channel>
</rss>