<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRCW QorIQ LS1043A</title>
    <link>https://community.nxp.com/t5/Layerscape/RCW-QorIQ-LS1043A/m-p/1361820#M9186</link>
    <description>&lt;P&gt;Hello everyone.&lt;/P&gt;&lt;P&gt;I have been trying to perform this task for several days.&lt;BR /&gt;Here is what I am doing:&lt;/P&gt;&lt;P&gt;&lt;FONT face="book antiqua,palatino"&gt;&lt;STRONG&gt;&lt;FONT size="5"&gt;Target:&lt;/FONT&gt;&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;My goal is to get my&amp;nbsp;&lt;STRONG&gt;QorIQ LS1043A&lt;/STRONG&gt; board&amp;nbsp;(multicore processor) to boot by SD and starting the core to run at 1.2GHz instead of 1.6GHz.&lt;/P&gt;&lt;P&gt;By default all four core of processor works at 1.6GHz. Once the system is up and running, i would like to see from U-boot that all core recive a frequency of 1.2GHz. Sometingh like this:&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF00FF"&gt;CPU0(A53):1200 MHz CPU1(A53):1200 MHz CPU2(A53):1200 MHz&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;CPU3(A53):1200 MHz&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;To generate the boot I am using flex-builder, in particular &lt;STRONG&gt;flexbuild_lsdk1712&lt;/STRONG&gt;. I saw from the documentation &lt;STRONG&gt;Layerscape Software Development Kit 17.12 Documentation, Rev. 0, 02/201&lt;/STRONG&gt; that it is possible to make the file&amp;nbsp;&lt;STRONG&gt;firmware_ls1043ardb_uboot_sdboot.img&amp;nbsp;&lt;/STRONG&gt;with the following command:&amp;nbsp;&lt;STRONG&gt;flex-builder -i mkfw -m ls1043ardb -b sd -B uboot.&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;&lt;STRONG&gt;I do this because I need to generate the boot from SD with U-Boot 2017 on it&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="book antiqua,palatino" size="5"&gt;&lt;STRONG&gt;Question:&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;The RCW to use to run the board at 1.2GHz is the following?&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;BR /&gt;0610000c 0a000000 00000000 00000000&lt;BR /&gt;14550002 80004012 60040000 c1002000&lt;BR /&gt;00000000 00000000 00000000 00038800&lt;BR /&gt;00000000 00001100 00000096 00000001&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have to go and replace the old RCW with the new one in the file&lt;STRONG&gt; ls1043ardb_rcw_sd.cfg&lt;/STRONG&gt;?&lt;/P&gt;&lt;P&gt;So inside the&amp;nbsp;&lt;STRONG&gt;ls1043ardb_rcw_sd.cfg&lt;/STRONG&gt; file there must be this:&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF00FF"&gt;#PBL preamble and RCW header&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;aa55aa55 01ee0100&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;# RCW&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;06100010 0a000000 00000000 00000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;14550002 80004012 60040000 c1002000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;00000000 00000000 00000000 00038800&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;00000000 00001100 00000096 00000001&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;the file is located in the following path: &lt;STRONG&gt;flexbuilder/packages/firmware/u-boot/board/freescale/ls1043ardb.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;By carrying out this procedure, the boot does not start.&lt;BR /&gt;everything is correct?&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;My default board starts with a core frequency of 1.6GHz, and 100MHz of SYSCLK.&lt;/FONT&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;Thank you very much for your availability.&lt;/P&gt;</description>
    <pubDate>Tue, 26 Oct 2021 15:52:27 GMT</pubDate>
    <dc:creator>notshure</dc:creator>
    <dc:date>2021-10-26T15:52:27Z</dc:date>
    <item>
      <title>RCW QorIQ LS1043A</title>
      <link>https://community.nxp.com/t5/Layerscape/RCW-QorIQ-LS1043A/m-p/1361820#M9186</link>
      <description>&lt;P&gt;Hello everyone.&lt;/P&gt;&lt;P&gt;I have been trying to perform this task for several days.&lt;BR /&gt;Here is what I am doing:&lt;/P&gt;&lt;P&gt;&lt;FONT face="book antiqua,palatino"&gt;&lt;STRONG&gt;&lt;FONT size="5"&gt;Target:&lt;/FONT&gt;&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;My goal is to get my&amp;nbsp;&lt;STRONG&gt;QorIQ LS1043A&lt;/STRONG&gt; board&amp;nbsp;(multicore processor) to boot by SD and starting the core to run at 1.2GHz instead of 1.6GHz.&lt;/P&gt;&lt;P&gt;By default all four core of processor works at 1.6GHz. Once the system is up and running, i would like to see from U-boot that all core recive a frequency of 1.2GHz. Sometingh like this:&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF00FF"&gt;CPU0(A53):1200 MHz CPU1(A53):1200 MHz CPU2(A53):1200 MHz&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;CPU3(A53):1200 MHz&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;To generate the boot I am using flex-builder, in particular &lt;STRONG&gt;flexbuild_lsdk1712&lt;/STRONG&gt;. I saw from the documentation &lt;STRONG&gt;Layerscape Software Development Kit 17.12 Documentation, Rev. 0, 02/201&lt;/STRONG&gt; that it is possible to make the file&amp;nbsp;&lt;STRONG&gt;firmware_ls1043ardb_uboot_sdboot.img&amp;nbsp;&lt;/STRONG&gt;with the following command:&amp;nbsp;&lt;STRONG&gt;flex-builder -i mkfw -m ls1043ardb -b sd -B uboot.&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;&lt;STRONG&gt;I do this because I need to generate the boot from SD with U-Boot 2017 on it&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="book antiqua,palatino" size="5"&gt;&lt;STRONG&gt;Question:&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;The RCW to use to run the board at 1.2GHz is the following?&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;BR /&gt;0610000c 0a000000 00000000 00000000&lt;BR /&gt;14550002 80004012 60040000 c1002000&lt;BR /&gt;00000000 00000000 00000000 00038800&lt;BR /&gt;00000000 00001100 00000096 00000001&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have to go and replace the old RCW with the new one in the file&lt;STRONG&gt; ls1043ardb_rcw_sd.cfg&lt;/STRONG&gt;?&lt;/P&gt;&lt;P&gt;So inside the&amp;nbsp;&lt;STRONG&gt;ls1043ardb_rcw_sd.cfg&lt;/STRONG&gt; file there must be this:&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF00FF"&gt;#PBL preamble and RCW header&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;aa55aa55 01ee0100&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;# RCW&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;06100010 0a000000 00000000 00000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;14550002 80004012 60040000 c1002000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;00000000 00000000 00000000 00038800&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;00000000 00001100 00000096 00000001&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;the file is located in the following path: &lt;STRONG&gt;flexbuilder/packages/firmware/u-boot/board/freescale/ls1043ardb.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;By carrying out this procedure, the boot does not start.&lt;BR /&gt;everything is correct?&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;My default board starts with a core frequency of 1.6GHz, and 100MHz of SYSCLK.&lt;/FONT&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;Thank you very much for your availability.&lt;/P&gt;</description>
      <pubDate>Tue, 26 Oct 2021 15:52:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/RCW-QorIQ-LS1043A/m-p/1361820#M9186</guid>
      <dc:creator>notshure</dc:creator>
      <dc:date>2021-10-26T15:52:27Z</dc:date>
    </item>
    <item>
      <title>Re: RCW QorIQ LS1043A</title>
      <link>https://community.nxp.com/t5/Layerscape/RCW-QorIQ-LS1043A/m-p/1362198#M9194</link>
      <description>&lt;P&gt;ls1043ardb_rcw_sd.cfg should be as the following.&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#FF00FF"&gt;#PBL preamble and RCW header&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;aa55aa55 01ee0100&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;# RCW&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;&lt;SPAN&gt;0610000c&lt;/SPAN&gt; 0a000000 00000000 00000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;14550002 80004012 60040000 c1002000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;00000000 00000000 00000000 00038800&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF00FF"&gt;00000000 00001100 00000096 00000001&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Oct 2021 07:27:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/RCW-QorIQ-LS1043A/m-p/1362198#M9194</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-10-27T07:27:05Z</dc:date>
    </item>
  </channel>
</rss>