<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1021A - RGMII eTSEC3, no 125MHz on EC3_GTX_CLK</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1021A-RGMII-eTSEC3-no-125MHz-on-EC3-GTX-CLK/m-p/486547#M917</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Problem was found to be improper termination on EC3_GTX_CLK125 clock source&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Feb 2016 21:11:33 GMT</pubDate>
    <dc:creator>Davisg</dc:creator>
    <dc:date>2016-02-03T21:11:33Z</dc:date>
    <item>
      <title>LS1021A - RGMII eTSEC3, no 125MHz on EC3_GTX_CLK</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-RGMII-eTSEC3-no-125MHz-on-EC3-GTX-CLK/m-p/486546#M916</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an LS1021A board designed by our customer that is configured for RGMII eTSEC3 using the same PHY (AR8033) as LS1021A-TWR board and connected exactly the same as the LS1021A-TWR board. Good 1Gbps link on Ethernet port. U-boot reports "Speed: 1000, full duplex" but fails ping with "not alive".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On LS1021A-TWR observe 125MHz clock on EC3_GTX_CLK when transmitting (ping from u-boot with "alive").&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On LS1021A board (not tower) there is no 125MHz clock on EC3_GTX_CLK when trying to transmit (ping from u-boot). There is activity on the EC3_GTX_CLK signal but it does not look like a clock (i.e., not 125MHz, 25MHz, or 2.5MHz clock).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have not been able to find what is causing this yet.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Feb 2016 17:35:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-RGMII-eTSEC3-no-125MHz-on-EC3-GTX-CLK/m-p/486546#M916</guid>
      <dc:creator>Davisg</dc:creator>
      <dc:date>2016-02-03T17:35:22Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021A - RGMII eTSEC3, no 125MHz on EC3_GTX_CLK</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-RGMII-eTSEC3-no-125MHz-on-EC3-GTX-CLK/m-p/486547#M917</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Problem was found to be improper termination on EC3_GTX_CLK125 clock source&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Feb 2016 21:11:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-RGMII-eTSEC3-no-125MHz-on-EC3-GTX-CLK/m-p/486547#M917</guid>
      <dc:creator>Davisg</dc:creator>
      <dc:date>2016-02-03T21:11:33Z</dc:date>
    </item>
  </channel>
</rss>