<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: Core disable on LS1043ardb</title>
    <link>https://community.nxp.com/t5/Layerscape/Core-disable-on-LS1043ardb/m-p/1352478#M9065</link>
    <description>&lt;P&gt;Thanks a lot for the answer.&lt;/P&gt;</description>
    <pubDate>Fri, 08 Oct 2021 07:54:09 GMT</pubDate>
    <dc:creator>notshure</dc:creator>
    <dc:date>2021-10-08T07:54:09Z</dc:date>
    <item>
      <title>Core disable on LS1043ardb</title>
      <link>https://community.nxp.com/t5/Layerscape/Core-disable-on-LS1043ardb/m-p/1351930#M9058</link>
      <description>&lt;P&gt;Hello to all, my goal is to get my &lt;STRONG&gt;LS1043a&lt;/STRONG&gt; board to boot by SD and starting the system by shutting down cores 1, 2 and 3. Once the system is up and running, i would like to see from uboot that such cores are disabled.&lt;/P&gt;&lt;P&gt;I performed a custom boot in which I entered the PBI command to disable the cores.&lt;/P&gt;&lt;P&gt;The procedure I followed is well described and can be found in the following link: &lt;A href="https://community.nxp.com/t5/Layerscape/Boot-problem-with-PBI/m-p/1350416#M9044" target="_self"&gt;Procedure&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm starting u-boot, and then so far so good.&lt;BR /&gt;But to make sure that the cores are off I went to read the DCFG_CCSR_COREDISR register, at the address 1EE_0094h using the following u-boot command:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;STRONG&gt;md 0x1ee0094 1&lt;/STRONG&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The result I get is the following:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;STRONG&gt;0x1ee0094: 0x0e000000&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I shouldn't be reading instead:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;STRONG&gt;0x1ee0094: 0x0000000e&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;since in the datasheet the bits of that register are defined in this way:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Cattura.PNG" style="width: 870px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/158480i12A587FC5AFB9DFE/image-size/large?v=v2&amp;amp;px=999" role="button" title="Cattura.PNG" alt="Cattura.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Oct 2021 13:18:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Core-disable-on-LS1043ardb/m-p/1351930#M9058</guid>
      <dc:creator>notshure</dc:creator>
      <dc:date>2021-10-07T13:18:49Z</dc:date>
    </item>
    <item>
      <title>Re: Core disable on LS1043ardb</title>
      <link>https://community.nxp.com/t5/Layerscape/Core-disable-on-LS1043ardb/m-p/1352086#M9062</link>
      <description>&lt;P&gt;U-Boot is natively big-endian, so for little-endian registers it is needed to perform byte swap.&lt;/P&gt;</description>
      <pubDate>Thu, 07 Oct 2021 17:56:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Core-disable-on-LS1043ardb/m-p/1352086#M9062</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-10-07T17:56:43Z</dc:date>
    </item>
    <item>
      <title>Re: Core disable on LS1043ardb</title>
      <link>https://community.nxp.com/t5/Layerscape/Core-disable-on-LS1043ardb/m-p/1352478#M9065</link>
      <description>&lt;P&gt;Thanks a lot for the answer.&lt;/P&gt;</description>
      <pubDate>Fri, 08 Oct 2021 07:54:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Core-disable-on-LS1043ardb/m-p/1352478#M9065</guid>
      <dc:creator>notshure</dc:creator>
      <dc:date>2021-10-08T07:54:09Z</dc:date>
    </item>
  </channel>
</rss>