<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 [lx2160a] About watchdog function ?</title>
    <link>https://community.nxp.com/t5/Layerscape/lx2160a-About-watchdog-function/m-p/1344869#M8960</link>
    <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;We enable LX2160A watchdog function in LSDK 2012 and do verification according to LSDK user guide.&lt;/P&gt;&lt;P&gt;We get the following message after pkill watchdog and wd_keepalive.&lt;/P&gt;&lt;P&gt;root@localhost:~# [ 305.595605] Kernel panic - not syncing: SBSA Generic Watchdog timeout&lt;BR /&gt;[ 305.602043] CPU: 0 PID: 0 Comm: swapper/0 Not tainted 5.4.47 #1&lt;BR /&gt;[ 305.607951] Hardware name: NXP Layerscape LX2160ARDB (DT)&lt;BR /&gt;[ 305.613339] Call trace:&lt;BR /&gt;[ 305.615781] dump_backtrace+0x0/0x150&lt;BR /&gt;[ 305.619434] show_stack+0x14/0x20&lt;BR /&gt;[ 305.622741] dump_stack+0xbc/0x100&lt;BR /&gt;[ 305.626133] panic+0x16c/0x37c&lt;BR /&gt;[ 305.629180] sbsa_gwdt_interrupt+0x14/0x18&lt;BR /&gt;[ 305.633267] __handle_irq_event_percpu+0x74/0x198&lt;BR /&gt;[ 305.637959] handle_irq_event_percpu+0x34/0x88&lt;BR /&gt;[ 305.642391] handle_irq_event+0x44/0xc8&lt;BR /&gt;[ 305.646217] handle_fasteoi_irq+0xac/0x150&lt;BR /&gt;[ 305.650304] generic_handle_irq+0x24/0x38&lt;BR /&gt;[ 305.654304] __handle_domain_irq+0x5c/0xb0&lt;BR /&gt;[ 305.658389] gic_handle_irq+0x5c/0x148&lt;BR /&gt;[ 305.662127] el1_irq+0xb8/0x180&lt;BR /&gt;[ 305.665259] cpuidle_enter_state+0x13c/0x340&lt;BR /&gt;[ 305.669518] cpuidle_enter+0x38/0x50&lt;BR /&gt;[ 305.673085] call_cpuidle+0x1c/0x40&lt;BR /&gt;[ 305.676562] do_idle+0x214/0x2b0&lt;BR /&gt;[ 305.679780] cpu_startup_entry+0x20/0x40&lt;BR /&gt;[ 305.683693] rest_init+0xd4/0xe0&lt;BR /&gt;[ 305.686913] arch_call_rest_init+0xc/0x14&lt;BR /&gt;[ 305.690911] start_kernel+0x424/0x458&lt;BR /&gt;[ 305.694576] SMP: stopping secondary CPUs&lt;BR /&gt;[ 305.698502] Kernel Offset: 0x264a79c00000 from 0xffff800010000000&lt;BR /&gt;[ 305.704583] PHYS_OFFSET: 0xffffe45280000000&lt;BR /&gt;[ 305.708756] CPU features: 0x0002,21806008&lt;BR /&gt;[ 305.712753] Memory Limit: none&lt;BR /&gt;[ 305.715807] ---[ end Kernel panic - not syncing: SBSA Generic Watchdog timeout ]---&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The result is correct?&lt;/P&gt;&lt;P&gt;In addition, we see watchdog NOTE indicates "SBSA watchdog on LX2160A will not reset the kernel but get kernel panic."&lt;/P&gt;&lt;P&gt;Does it mean LX2160A reset system by watchdog is not available ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jeffrey&lt;/P&gt;</description>
    <pubDate>Thu, 23 Sep 2021 08:18:14 GMT</pubDate>
    <dc:creator>Jeffrey_Lai</dc:creator>
    <dc:date>2021-09-23T08:18:14Z</dc:date>
    <item>
      <title>[lx2160a] About watchdog function ?</title>
      <link>https://community.nxp.com/t5/Layerscape/lx2160a-About-watchdog-function/m-p/1344869#M8960</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;We enable LX2160A watchdog function in LSDK 2012 and do verification according to LSDK user guide.&lt;/P&gt;&lt;P&gt;We get the following message after pkill watchdog and wd_keepalive.&lt;/P&gt;&lt;P&gt;root@localhost:~# [ 305.595605] Kernel panic - not syncing: SBSA Generic Watchdog timeout&lt;BR /&gt;[ 305.602043] CPU: 0 PID: 0 Comm: swapper/0 Not tainted 5.4.47 #1&lt;BR /&gt;[ 305.607951] Hardware name: NXP Layerscape LX2160ARDB (DT)&lt;BR /&gt;[ 305.613339] Call trace:&lt;BR /&gt;[ 305.615781] dump_backtrace+0x0/0x150&lt;BR /&gt;[ 305.619434] show_stack+0x14/0x20&lt;BR /&gt;[ 305.622741] dump_stack+0xbc/0x100&lt;BR /&gt;[ 305.626133] panic+0x16c/0x37c&lt;BR /&gt;[ 305.629180] sbsa_gwdt_interrupt+0x14/0x18&lt;BR /&gt;[ 305.633267] __handle_irq_event_percpu+0x74/0x198&lt;BR /&gt;[ 305.637959] handle_irq_event_percpu+0x34/0x88&lt;BR /&gt;[ 305.642391] handle_irq_event+0x44/0xc8&lt;BR /&gt;[ 305.646217] handle_fasteoi_irq+0xac/0x150&lt;BR /&gt;[ 305.650304] generic_handle_irq+0x24/0x38&lt;BR /&gt;[ 305.654304] __handle_domain_irq+0x5c/0xb0&lt;BR /&gt;[ 305.658389] gic_handle_irq+0x5c/0x148&lt;BR /&gt;[ 305.662127] el1_irq+0xb8/0x180&lt;BR /&gt;[ 305.665259] cpuidle_enter_state+0x13c/0x340&lt;BR /&gt;[ 305.669518] cpuidle_enter+0x38/0x50&lt;BR /&gt;[ 305.673085] call_cpuidle+0x1c/0x40&lt;BR /&gt;[ 305.676562] do_idle+0x214/0x2b0&lt;BR /&gt;[ 305.679780] cpu_startup_entry+0x20/0x40&lt;BR /&gt;[ 305.683693] rest_init+0xd4/0xe0&lt;BR /&gt;[ 305.686913] arch_call_rest_init+0xc/0x14&lt;BR /&gt;[ 305.690911] start_kernel+0x424/0x458&lt;BR /&gt;[ 305.694576] SMP: stopping secondary CPUs&lt;BR /&gt;[ 305.698502] Kernel Offset: 0x264a79c00000 from 0xffff800010000000&lt;BR /&gt;[ 305.704583] PHYS_OFFSET: 0xffffe45280000000&lt;BR /&gt;[ 305.708756] CPU features: 0x0002,21806008&lt;BR /&gt;[ 305.712753] Memory Limit: none&lt;BR /&gt;[ 305.715807] ---[ end Kernel panic - not syncing: SBSA Generic Watchdog timeout ]---&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The result is correct?&lt;/P&gt;&lt;P&gt;In addition, we see watchdog NOTE indicates "SBSA watchdog on LX2160A will not reset the kernel but get kernel panic."&lt;/P&gt;&lt;P&gt;Does it mean LX2160A reset system by watchdog is not available ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jeffrey&lt;/P&gt;</description>
      <pubDate>Thu, 23 Sep 2021 08:18:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/lx2160a-About-watchdog-function/m-p/1344869#M8960</guid>
      <dc:creator>Jeffrey_Lai</dc:creator>
      <dc:date>2021-09-23T08:18:14Z</dc:date>
    </item>
  </channel>
</rss>