<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Processor LS1043a Linux network driver consulting in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Processor-LS1043a-Linux-network-driver-consulting/m-p/1339409#M8903</link>
    <description>&lt;P&gt;&lt;SPAN&gt;LS1043A is dpaa based, so only dpaa+fman drivers are valid. And sdk_dpaa+sdk_fman drivers are for Linux kernel in LSDK, dpaa+fman drive are for upstream Linux kernel use. Besides the sdk_dpaa+sdk_fman driver, you are supposed to use fsl-ls1043a-rdb-sdk.dts for LSDK Kernel use.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 14 Sep 2021 03:14:45 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2021-09-14T03:14:45Z</dc:date>
    <item>
      <title>Processor LS1043a Linux network driver consulting</title>
      <link>https://community.nxp.com/t5/Layerscape/Processor-LS1043a-Linux-network-driver-consulting/m-p/1336716#M8865</link>
      <description>&lt;P&gt;There is a project using the processor LS1043a. The Linux version is 5.4.3. The directory drivers\net\ethernet\freescale has network drivers. As shown below:&lt;/P&gt;&lt;P&gt;dpaa&lt;/P&gt;&lt;P&gt;dpaa2&lt;/P&gt;&lt;P&gt;enetc&lt;/P&gt;&lt;P&gt;fman&lt;/P&gt;&lt;P&gt;fs_enet&lt;/P&gt;&lt;P&gt;sdk_dpaa&lt;/P&gt;&lt;P&gt;sdk_fman&lt;/P&gt;&lt;P&gt;What is the difference between the drivers in these subdirectories. especially the difference between the sdk_dpaa and sdk_fman directories.&lt;/P&gt;</description>
      <pubDate>Wed, 08 Sep 2021 08:30:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Processor-LS1043a-Linux-network-driver-consulting/m-p/1336716#M8865</guid>
      <dc:creator>niehy</dc:creator>
      <dc:date>2021-09-08T08:30:36Z</dc:date>
    </item>
    <item>
      <title>Re: Processor LS1043a Linux network driver consulting</title>
      <link>https://community.nxp.com/t5/Layerscape/Processor-LS1043a-Linux-network-driver-consulting/m-p/1339409#M8903</link>
      <description>&lt;P&gt;&lt;SPAN&gt;LS1043A is dpaa based, so only dpaa+fman drivers are valid. And sdk_dpaa+sdk_fman drivers are for Linux kernel in LSDK, dpaa+fman drive are for upstream Linux kernel use. Besides the sdk_dpaa+sdk_fman driver, you are supposed to use fsl-ls1043a-rdb-sdk.dts for LSDK Kernel use.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Sep 2021 03:14:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Processor-LS1043a-Linux-network-driver-consulting/m-p/1339409#M8903</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-09-14T03:14:45Z</dc:date>
    </item>
  </channel>
</rss>