<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックAbout PCI Express lanes</title>
    <link>https://community.nxp.com/t5/Layerscape/About-PCI-Express-lanes/m-p/1336464#M8862</link>
    <description>&lt;P&gt;Hi There,&lt;/P&gt;&lt;P&gt;We plan to use the LS1043A for in Automotive use.&lt;BR /&gt;Use SerDes with SRDS_PRTCL_S1 = 9960.&lt;BR /&gt;(A:PCIe(x1)、B:PCIe(x1)、C/D:PCIe(x2))&lt;BR /&gt;I want to run an SSD module (PCIex4) with SerDes C/D.&lt;/P&gt;&lt;P&gt;I have some questions on the "LS1043A".&lt;/P&gt;&lt;P&gt;1.Are SerDes C = lane0 and SerDes D = lane1 correct ?&lt;/P&gt;&lt;P&gt;2.Does the PCI controller support 2-lane operation ?&lt;BR /&gt;(SSD module (PCIe x 4))&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;- satoshi&lt;/P&gt;</description>
    <pubDate>Wed, 08 Sep 2021 04:30:52 GMT</pubDate>
    <dc:creator>okamotosatoshi</dc:creator>
    <dc:date>2021-09-08T04:30:52Z</dc:date>
    <item>
      <title>About PCI Express lanes</title>
      <link>https://community.nxp.com/t5/Layerscape/About-PCI-Express-lanes/m-p/1336464#M8862</link>
      <description>&lt;P&gt;Hi There,&lt;/P&gt;&lt;P&gt;We plan to use the LS1043A for in Automotive use.&lt;BR /&gt;Use SerDes with SRDS_PRTCL_S1 = 9960.&lt;BR /&gt;(A:PCIe(x1)、B:PCIe(x1)、C/D:PCIe(x2))&lt;BR /&gt;I want to run an SSD module (PCIex4) with SerDes C/D.&lt;/P&gt;&lt;P&gt;I have some questions on the "LS1043A".&lt;/P&gt;&lt;P&gt;1.Are SerDes C = lane0 and SerDes D = lane1 correct ?&lt;/P&gt;&lt;P&gt;2.Does the PCI controller support 2-lane operation ?&lt;BR /&gt;(SSD module (PCIe x 4))&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;- satoshi&lt;/P&gt;</description>
      <pubDate>Wed, 08 Sep 2021 04:30:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/About-PCI-Express-lanes/m-p/1336464#M8862</guid>
      <dc:creator>okamotosatoshi</dc:creator>
      <dc:date>2021-09-08T04:30:52Z</dc:date>
    </item>
    <item>
      <title>Re: About PCI Express lanes</title>
      <link>https://community.nxp.com/t5/Layerscape/About-PCI-Express-lanes/m-p/1339363#M8901</link>
      <description>&lt;OL&gt;
&lt;LI&gt;&lt;SPAN&gt; Are SerDes C = lane0 and SerDes D = lane1 correct ?&lt;/SPAN&gt;&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;&lt;SPAN&gt;[NXP] LNmGCR0[FIRST_LANE] --&amp;gt; Indicates the lane is the first (lane 0) of a group of lanes. For the 0x9960 protocol, you will see the value for Lane C as 1'b1 indicating lane 0 of the link, whereas, for lane D, the value will be 1'b0, indicating NOT lane 0 of the link. &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;OL start="2"&gt;
&lt;LI&gt;&lt;SPAN&gt; Does the PCI controller support a 2-lane operation?&lt;/SPAN&gt;&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;&lt;SPAN&gt;(SSD module (PCIe x 4))&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;[NXP] Yes, it should work assuming SSD is connected via the SATA-PCIe interface.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Sep 2021 01:49:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/About-PCI-Express-lanes/m-p/1339363#M8901</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-09-14T01:49:24Z</dc:date>
    </item>
  </channel>
</rss>