<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Parameters to reduce SDRAM power consomption</title>
    <link>https://community.nxp.com/t5/Layerscape/Parameters-to-reduce-SDRAM-power-consomption/m-p/1336230#M8856</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The 'DDR memory controller' allows us to choose the 'power management mode'.&lt;/P&gt;&lt;P&gt;In the 'QorIQ LS1028A Reference Manual', I read the 'dynamic power management mode' can reduce power consomption.&lt;/P&gt;&lt;P&gt;My first question is:&lt;/P&gt;&lt;P&gt;does this mode reduce the DDR refresh rate, and is there an impact about the performances?&lt;/P&gt;&lt;P&gt;My second question is how to active this 'power management mode'? Is there a regsiter to write in it, at which step of the boot (with the PreBoot Loader ?)?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;</description>
    <pubDate>Tue, 07 Sep 2021 16:24:12 GMT</pubDate>
    <dc:creator>mbourhis</dc:creator>
    <dc:date>2021-09-07T16:24:12Z</dc:date>
    <item>
      <title>Parameters to reduce SDRAM power consomption</title>
      <link>https://community.nxp.com/t5/Layerscape/Parameters-to-reduce-SDRAM-power-consomption/m-p/1336230#M8856</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The 'DDR memory controller' allows us to choose the 'power management mode'.&lt;/P&gt;&lt;P&gt;In the 'QorIQ LS1028A Reference Manual', I read the 'dynamic power management mode' can reduce power consomption.&lt;/P&gt;&lt;P&gt;My first question is:&lt;/P&gt;&lt;P&gt;does this mode reduce the DDR refresh rate, and is there an impact about the performances?&lt;/P&gt;&lt;P&gt;My second question is how to active this 'power management mode'? Is there a regsiter to write in it, at which step of the boot (with the PreBoot Loader ?)?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Tue, 07 Sep 2021 16:24:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Parameters-to-reduce-SDRAM-power-consomption/m-p/1336230#M8856</guid>
      <dc:creator>mbourhis</dc:creator>
      <dc:date>2021-09-07T16:24:12Z</dc:date>
    </item>
    <item>
      <title>Re: Parameters to reduce SDRAM power consomption</title>
      <link>https://community.nxp.com/t5/Layerscape/Parameters-to-reduce-SDRAM-power-consomption/m-p/1336480#M8864</link>
      <description>&lt;P&gt;1. When dynamic power management mode is enabled, it puts SDRAM devices into power-down mode when there is no ongoing memory activity by negating CKE signal. Details of 'power-down mode' can be found in SDRAM datasheets.&lt;/P&gt;
&lt;P&gt;When the memory exits from the power-down mode, it requires some time delay (tXP) before any bus command (like read/write), so yes, this mode slightly affects performance.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2. To enable dynamic power management mode the user should set bit DDR_SDRAM_CFG[DYN_PWR]. This can be done any time, for example before the DDR controller is enabled.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Bulat&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Sep 2021 05:06:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Parameters-to-reduce-SDRAM-power-consomption/m-p/1336480#M8864</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2021-09-08T05:06:45Z</dc:date>
    </item>
  </channel>
</rss>