<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: PCIe NVMe SSD Not recognised</title>
    <link>https://community.nxp.com/t5/Layerscape/PCIe-NVMe-SSD-Not-recognised/m-p/483873#M882</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It turns out that the PBL binary file supplied with the Freescale Yocto project does not work for the LS2085A board (please bear in mind I have a LS2085A that I am configuring to behave as a LS2080A).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When doing the Yocto build for the ls2080ardb, I get a folder:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;build_ls2080ardb_release/tmp/deploy/images/ls2080ardb/rcw/rcw_0x2a_0x41/PBL_0x2a_0x41_1867_533_1867.bin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I upload this onto the board by interrupting uboot in vbank0, following the LS2080A SDK 1.0 Deployment Guide:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; tftp 0x80000000 PBL_0x2a_0x41_1867_533_1867.bin; erase 0x585400000 +$filesize; cp.b 0x80000000 0x585400000 $filesize&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I then reboot into vbank4:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; qixis_reset altbank&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I am booting into vbank4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the Yocto Project PBL_0x2a_0x41_1867_533_1867.bin, the NVMe SSD is not recognised. In the u-boot output I see something like:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PCIe1: disabled&lt;/P&gt;&lt;P&gt;PCIe2: disabled&lt;/P&gt;&lt;P&gt;PCIe3: Root Complex no link, regs @ 0x3600000&lt;/P&gt;&lt;P&gt;PCIe4: Root Complex no link, regs @ 0x3700000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Following &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/ufedor"&gt;ufedor&lt;/A&gt;​'s suggestion, I opened the PBL file in QCVS. I created a new QorIQ configuration project for the LS2085A and in the SerDes blocks I selected the following checkbox options: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- enable SATA-&amp;gt;1.5&lt;/P&gt;&lt;P&gt;- enable XFI-&amp;gt;10.3125&lt;/P&gt;&lt;P&gt;- enable SGMII-&amp;gt;1.25&lt;/P&gt;&lt;P&gt;- enable PCIe-&amp;gt;Gen1 2.5&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I then selected&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0x2A for SerDes1: XFI1-8=10.3125, PLL=11111111)&lt;/P&gt;&lt;P&gt;0x41 for SerDes2: PCIe3 (2.5), 4 lanes; PCIe4 (2.5), 2 lanes; SATA1(1.5) 1 lane;&amp;nbsp; SATA2(1.5) 1 lane&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So nominally, the protocols are the same as those specified in the Yocto Project PBL file. I created a PBL file with this configuration and uploaded it to the LS2085A as aboce. When I boot into vbank4, uboot now looks like this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PCIe1: disabled&lt;/P&gt;&lt;P&gt;PCIe2: disabled&lt;/P&gt;&lt;P&gt;PCIe3: Root Complex x4 gen2, regs @ 0x3600000&lt;/P&gt;&lt;P&gt;PCI:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 01:00.0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - 8086:0953 - Mass storage controller&lt;/P&gt;&lt;P&gt;PCIe3: Bus 00 - 01&lt;/P&gt;&lt;P&gt;PCIe4: Root Complex x2 gen2, regs @ 0x3700000&lt;/P&gt;&lt;P&gt;PCI:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 03:00.0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - 144d:a802 - Mass storage controller&lt;/P&gt;&lt;P&gt;PCIe4: Bus 02 - 03&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(note that for fun I put two NVMe disks in). The NVMe disk is recognised with the correct PCI vendor and device IDs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The difference between the PBL file from Yocto and the one from QCVS was different SERDES PLL and Protocol Configuration (Bits 911-896) and settings for the Layerscape Chassis EXPANSION AREA (Bits 1023-912) (see the QCVS Component Inspector - PBL Properties tab for the PBL file).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the Yocto project PBL, SRDS_PLL_PD_PLL2 was not powered down (0b0) and SRDS_DIV_PEX_S2 was set to 0b00 (up to max rate of 8G). If these are set to 0b1 and 0b10/0b01 respectively, the NVMe drive is recognised.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 May 2016 09:55:58 GMT</pubDate>
    <dc:creator>thomasculverhou</dc:creator>
    <dc:date>2016-05-27T09:55:58Z</dc:date>
    <item>
      <title>PCIe NVMe SSD Not recognised</title>
      <link>https://community.nxp.com/t5/Layerscape/PCIe-NVMe-SSD-Not-recognised/m-p/483868#M877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a Freescale LS2080 box for which I am developing a custom linux 4.1.8 kernel using the Freescale Yocto project.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an NVMe hard disk attached to the LS2080 via a PCIe card, but the disk is not recognised when I boot up the board with my custom linux kernel.&amp;nbsp; In fact, it is not recognised in u-boot either if I do &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt; pci&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I plugged the same combination of NVMe disk and PCIe card into a Debian linux 3.16.7 desktop PC and it was detected and mounted without problem.&amp;nbsp; I also repeated the experiment with a different PCIe card and different NVMe SSD and got the same result.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When building the LS2080 kernel using the Yocto project, I have enabled the NVMe block device driver and I have verified that this module is present in the kernel when booting on the board.&amp;nbsp; The PCIe slot on the board is working fine because I have tried it with a PCIe Ethernet card and a PCIe SATA disk.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only thing I can think of is that the Ethernet card is 1x lane PCIe device, and the SATA disk is 2x lanes, while the NVMe is 4x lanes - perhaps the 4x lanes aren't working on the board, or the DIP switches are set incorrectly?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect that I am missing something in the kernel configuration or device tree, but I'm not sure what. When I add the NVMe driver to the kernel using menuconfig, the NVMe driver dependencies are supposed to be resolved.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone provide insight into what I am missing?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 May 2016 07:44:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PCIe-NVMe-SSD-Not-recognised/m-p/483868#M877</guid>
      <dc:creator>thomasculverhou</dc:creator>
      <dc:date>2016-05-19T07:44:45Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe NVMe SSD Not recognised</title>
      <link>https://community.nxp.com/t5/Layerscape/PCIe-NVMe-SSD-Not-recognised/m-p/483869#M878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please provide U-Boot booting log when the PCIe card is inserted.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 May 2016 11:52:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PCIe-NVMe-SSD-Not-recognised/m-p/483869#M878</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-05-19T11:52:09Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe NVMe SSD Not recognised</title>
      <link>https://community.nxp.com/t5/Layerscape/PCIe-NVMe-SSD-Not-recognised/m-p/483870#M879</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is booting using u-boot present on the board when it arrived (vbank0; the result is the same when I boot using u-boot compiled from the Yocto project and loaded to vbank4 NOR FLASH):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2015.01Layerscape2-SDK+g16c10aa (May 14 2015 - 15:17:11)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SoC:&amp;nbsp; LS2085E (0x87010010)&lt;/P&gt;&lt;P&gt;Clock Configuration:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CPU0(A57):1800 MHz&amp;nbsp; CPU1(A57):1800 MHz&amp;nbsp; CPU2(A57):1800 MHz&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CPU3(A57):1800 MHz&amp;nbsp; CPU4(A57):1800 MHz&amp;nbsp; CPU5(A57):1800 MHz&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CPU6(A57):1800 MHz&amp;nbsp; CPU7(A57):1800 MHz&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Bus:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 600&amp;nbsp; MHz&amp;nbsp; DDR:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1866.667 MT/s&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DP-DDR:&amp;nbsp;&amp;nbsp; 1600 MT/s&lt;/P&gt;&lt;P&gt;Reset Configuration Word (RCW):&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 00: 48303830 48480048 00000000 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 10: 00000000 00200000 00200000 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 20: 00c12980 00002580 00000000 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 30: 00000e0b 00000000 00000000 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 40: 00000000 00000000 00000000 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 50: 00000000 00000000 00000000 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 60: 00000000 00000000 00027000 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 70: 412a0000 00000000 00000000 00000000&lt;/P&gt;&lt;P&gt;Board: LS2085E-RDB, Board Arch: V1, Board version: D, boot from vBank: 0&lt;/P&gt;&lt;P&gt;FPGA: v1.18&lt;/P&gt;&lt;P&gt;SERDES1 Reference : Clock1 = 156.25MHz Clock2 = 156.25MHz&lt;/P&gt;&lt;P&gt;SERDES2 Reference : Clock1 = 100MHz Clock2 = 100MHz&lt;/P&gt;&lt;P&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;/P&gt;&lt;P&gt;DRAM:&amp;nbsp; Initializing DDR....using SPD&lt;/P&gt;&lt;P&gt;Detected UDIMM 18ASF1G72AZ-2G1A1&lt;/P&gt;&lt;P&gt;Detected UDIMM 18ASF1G72AZ-2G1A1&lt;/P&gt;&lt;P&gt;DP-DDR:&amp;nbsp; Detected UDIMM 18ASF1G72AZ-2G1A1&lt;/P&gt;&lt;P&gt;19.5 GiB&lt;/P&gt;&lt;P&gt;DDR&amp;nbsp;&amp;nbsp;&amp;nbsp; 15.5 GiB (DDR4, 64-bit, CL=13, ECC on)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DDR Controller Interleaving Mode: 256B&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DDR Chip-Select Interleaving Mode: CS0+CS1&lt;/P&gt;&lt;P&gt;DP-DDR 4 GiB (DDR4, 32-bit, CL=11, ECC on)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DDR Chip-Select Interleaving Mode: CS0+CS1&lt;/P&gt;&lt;P&gt;Waking secondary cores to start from fff1b000&lt;/P&gt;&lt;P&gt;All (8) cores are up.&lt;/P&gt;&lt;P&gt;Using SERDES1 Protocol: 42 (0x2a)&lt;/P&gt;&lt;P&gt;Using SERDES2 Protocol: 65 (0x41)&lt;/P&gt;&lt;P&gt;Flash: 128 MiB&lt;/P&gt;&lt;P&gt;NAND:&amp;nbsp; 2048 MiB&lt;/P&gt;&lt;P&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0&lt;/P&gt;&lt;P&gt;EEPROM: Invalid ID (ff ff ff ff)&lt;/P&gt;&lt;P&gt;PCIe1: disabled&lt;/P&gt;&lt;P&gt;PCIe2: disabled&lt;/P&gt;&lt;P&gt;PCIe3: Root Complex no link, regs @ 0x3600000&lt;/P&gt;&lt;P&gt;PCIe4: Root Complex no link, regs @ 0x3700000&lt;/P&gt;&lt;P&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Error! Not a FIT image&lt;/P&gt;&lt;P&gt;SATA link 0 timeout.&lt;/P&gt;&lt;P&gt;AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl SATA mode&lt;/P&gt;&lt;P&gt;flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst&lt;/P&gt;&lt;P&gt;Found 0 device(s).&lt;/P&gt;&lt;P&gt;SCSI:&amp;nbsp; Net:&amp;nbsp;&amp;nbsp; crc32+&lt;/P&gt;&lt;P&gt;fsl-mc: Booting Management Complex ... SUCCESS&lt;/P&gt;&lt;P&gt;fsl-mc: Management Complex booted (version: 7.0.3, boot status: 0x1)&lt;/P&gt;&lt;P&gt;fsl-mc: Deploying data path layout ... SUCCESS&lt;/P&gt;&lt;P&gt;DPNI10, DPNI8&lt;/P&gt;&lt;P&gt;Error: DPNI8 address not set.&lt;/P&gt;&lt;P&gt;, DPNI1, DPNI2&lt;/P&gt;&lt;P&gt;Error: DPNI2 address not set.&lt;/P&gt;&lt;P&gt;, DPNI3&lt;/P&gt;&lt;P&gt;Error: DPNI3 address not set.&lt;/P&gt;&lt;P&gt;, DPNI4&lt;/P&gt;&lt;P&gt;Error: DPNI4 address not set.&lt;/P&gt;&lt;P&gt;, DPNI7, DPNI9&lt;/P&gt;&lt;P&gt;Error: DPNI9 address not set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot:&amp;nbsp; 0 &lt;/P&gt;&lt;P&gt;=&amp;gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I insert e.g. a network card into the same PCIe slot, I get this in the PCIe section of u-boot output:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PCIe1: disabled&lt;/P&gt;&lt;P&gt;PCIe2: disabled&lt;/P&gt;&lt;P&gt;PCIe3: Root Complex x1 gen1, regs @ 0x3600000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 01:00.0&amp;nbsp;&amp;nbsp;&amp;nbsp; - 8086:10d3 - Network controller&lt;/P&gt;&lt;P&gt;PCIe3: Bus 00 - 01&lt;/P&gt;&lt;P&gt;PCIe4: Root Complex no link, regs @ 0x3700000&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 May 2016 13:11:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PCIe-NVMe-SSD-Not-recognised/m-p/483870#M879</guid>
      <dc:creator>thomasculverhou</dc:creator>
      <dc:date>2016-05-19T13:11:02Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe NVMe SSD Not recognised</title>
      <link>https://community.nxp.com/t5/Layerscape/PCIe-NVMe-SSD-Not-recognised/m-p/483871#M880</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As a side note, in the u-boot source code tmp/work/ls2080ardb-fsl-linux/u-boot-ls2/2015.10+fslgit-r0/git/include/pci_ids.h, I notice that the NVMe storage is not represented at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The class ID is defined in the kernel source code tmp/work-shared/ls2080ardb/kernel-source/drivers/block/nvme-core.c: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define PCI_CLASS_STORAGE_EXPRESS 0x010802&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is not present in the u-boot source code - perhaps this explains why the device is not recognised in u-boot?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 May 2016 14:22:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PCIe-NVMe-SSD-Not-recognised/m-p/483871#M880</guid>
      <dc:creator>thomasculverhou</dc:creator>
      <dc:date>2016-05-19T14:22:34Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe NVMe SSD Not recognised</title>
      <link>https://community.nxp.com/t5/Layerscape/PCIe-NVMe-SSD-Not-recognised/m-p/483872#M881</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The issue could be a complicated one.&lt;/P&gt;&lt;P&gt;In this case it is recommended to create a technical case - &lt;A href="https://community.nxp.com/thread/381898"&gt;How I could create a Service Request?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;During the case creation please provide additional information: company name, project phase and application type.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 May 2016 01:32:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PCIe-NVMe-SSD-Not-recognised/m-p/483872#M881</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-05-20T01:32:09Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe NVMe SSD Not recognised</title>
      <link>https://community.nxp.com/t5/Layerscape/PCIe-NVMe-SSD-Not-recognised/m-p/483873#M882</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It turns out that the PBL binary file supplied with the Freescale Yocto project does not work for the LS2085A board (please bear in mind I have a LS2085A that I am configuring to behave as a LS2080A).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When doing the Yocto build for the ls2080ardb, I get a folder:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;build_ls2080ardb_release/tmp/deploy/images/ls2080ardb/rcw/rcw_0x2a_0x41/PBL_0x2a_0x41_1867_533_1867.bin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I upload this onto the board by interrupting uboot in vbank0, following the LS2080A SDK 1.0 Deployment Guide:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; tftp 0x80000000 PBL_0x2a_0x41_1867_533_1867.bin; erase 0x585400000 +$filesize; cp.b 0x80000000 0x585400000 $filesize&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I then reboot into vbank4:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; qixis_reset altbank&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I am booting into vbank4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the Yocto Project PBL_0x2a_0x41_1867_533_1867.bin, the NVMe SSD is not recognised. In the u-boot output I see something like:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PCIe1: disabled&lt;/P&gt;&lt;P&gt;PCIe2: disabled&lt;/P&gt;&lt;P&gt;PCIe3: Root Complex no link, regs @ 0x3600000&lt;/P&gt;&lt;P&gt;PCIe4: Root Complex no link, regs @ 0x3700000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Following &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/ufedor"&gt;ufedor&lt;/A&gt;​'s suggestion, I opened the PBL file in QCVS. I created a new QorIQ configuration project for the LS2085A and in the SerDes blocks I selected the following checkbox options: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- enable SATA-&amp;gt;1.5&lt;/P&gt;&lt;P&gt;- enable XFI-&amp;gt;10.3125&lt;/P&gt;&lt;P&gt;- enable SGMII-&amp;gt;1.25&lt;/P&gt;&lt;P&gt;- enable PCIe-&amp;gt;Gen1 2.5&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I then selected&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0x2A for SerDes1: XFI1-8=10.3125, PLL=11111111)&lt;/P&gt;&lt;P&gt;0x41 for SerDes2: PCIe3 (2.5), 4 lanes; PCIe4 (2.5), 2 lanes; SATA1(1.5) 1 lane;&amp;nbsp; SATA2(1.5) 1 lane&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So nominally, the protocols are the same as those specified in the Yocto Project PBL file. I created a PBL file with this configuration and uploaded it to the LS2085A as aboce. When I boot into vbank4, uboot now looks like this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PCIe1: disabled&lt;/P&gt;&lt;P&gt;PCIe2: disabled&lt;/P&gt;&lt;P&gt;PCIe3: Root Complex x4 gen2, regs @ 0x3600000&lt;/P&gt;&lt;P&gt;PCI:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 01:00.0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - 8086:0953 - Mass storage controller&lt;/P&gt;&lt;P&gt;PCIe3: Bus 00 - 01&lt;/P&gt;&lt;P&gt;PCIe4: Root Complex x2 gen2, regs @ 0x3700000&lt;/P&gt;&lt;P&gt;PCI:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 03:00.0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - 144d:a802 - Mass storage controller&lt;/P&gt;&lt;P&gt;PCIe4: Bus 02 - 03&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(note that for fun I put two NVMe disks in). The NVMe disk is recognised with the correct PCI vendor and device IDs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The difference between the PBL file from Yocto and the one from QCVS was different SERDES PLL and Protocol Configuration (Bits 911-896) and settings for the Layerscape Chassis EXPANSION AREA (Bits 1023-912) (see the QCVS Component Inspector - PBL Properties tab for the PBL file).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the Yocto project PBL, SRDS_PLL_PD_PLL2 was not powered down (0b0) and SRDS_DIV_PEX_S2 was set to 0b00 (up to max rate of 8G). If these are set to 0b1 and 0b10/0b01 respectively, the NVMe drive is recognised.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 May 2016 09:55:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PCIe-NVMe-SSD-Not-recognised/m-p/483873#M882</guid>
      <dc:creator>thomasculverhou</dc:creator>
      <dc:date>2016-05-27T09:55:58Z</dc:date>
    </item>
  </channel>
</rss>