<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックLS1046A boundary scan register TDR layout</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046A-boundary-scan-register-TDR-layout/m-p/1330126#M8775</link>
    <description>&lt;P&gt;I need to set the TDR register via the IOCONFIG command, but can not find the register layout.&lt;BR /&gt;I have read the AN5352 application note, but it is for another CPU with register length of 105, LS1046A has a register length of 162.&lt;BR /&gt;BR Lars Thestrup&lt;/P&gt;</description>
    <pubDate>Thu, 26 Aug 2021 07:44:11 GMT</pubDate>
    <dc:creator>larsthestrup</dc:creator>
    <dc:date>2021-08-26T07:44:11Z</dc:date>
    <item>
      <title>LS1046A boundary scan register TDR layout</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-boundary-scan-register-TDR-layout/m-p/1330126#M8775</link>
      <description>&lt;P&gt;I need to set the TDR register via the IOCONFIG command, but can not find the register layout.&lt;BR /&gt;I have read the AN5352 application note, but it is for another CPU with register length of 105, LS1046A has a register length of 162.&lt;BR /&gt;BR Lars Thestrup&lt;/P&gt;</description>
      <pubDate>Thu, 26 Aug 2021 07:44:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-boundary-scan-register-TDR-layout/m-p/1330126#M8775</guid>
      <dc:creator>larsthestrup</dc:creator>
      <dc:date>2021-08-26T07:44:11Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A boundary scan register TDR layout</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-boundary-scan-register-TDR-layout/m-p/1330302#M8778</link>
      <description>&lt;P&gt;Please refer to the AN5378:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN5378" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=AN5378&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Aug 2021 10:45:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-boundary-scan-register-TDR-layout/m-p/1330302#M8778</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-08-26T10:45:45Z</dc:date>
    </item>
  </channel>
</rss>