<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic No messages from UART in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/No-messages-from-UART/m-p/1319718#M8667</link>
    <description>&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;I have LS1046A-RDB and I cannot boot it up. There is no UART messages. I've tried both options (micro-USB and RJ-45). This happened after failing to flash the QSPI firmware for another board (FRWY-1046) using the quick start guide as shown below.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="maksimdemin_0-1628255202656.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/152145i1F334E7822C7262D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="maksimdemin_0-1628255202656.png" alt="maksimdemin_0-1628255202656.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;maksimdemin_0-1628255202656.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help is appreciated. Thanks!&lt;/P&gt;</description>
    <pubDate>Fri, 06 Aug 2021 13:14:35 GMT</pubDate>
    <dc:creator>maksimdemin</dc:creator>
    <dc:date>2021-08-06T13:14:35Z</dc:date>
    <item>
      <title>No messages from UART</title>
      <link>https://community.nxp.com/t5/Layerscape/No-messages-from-UART/m-p/1319718#M8667</link>
      <description>&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;I have LS1046A-RDB and I cannot boot it up. There is no UART messages. I've tried both options (micro-USB and RJ-45). This happened after failing to flash the QSPI firmware for another board (FRWY-1046) using the quick start guide as shown below.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="maksimdemin_0-1628255202656.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/152145i1F334E7822C7262D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="maksimdemin_0-1628255202656.png" alt="maksimdemin_0-1628255202656.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;maksimdemin_0-1628255202656.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help is appreciated. Thanks!&lt;/P&gt;</description>
      <pubDate>Fri, 06 Aug 2021 13:14:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/No-messages-from-UART/m-p/1319718#M8667</guid>
      <dc:creator>maksimdemin</dc:creator>
      <dc:date>2021-08-06T13:14:35Z</dc:date>
    </item>
    <item>
      <title>Re: No messages from UART</title>
      <link>https://community.nxp.com/t5/Layerscape/No-messages-from-UART/m-p/1319928#M8672</link>
      <description>&lt;P&gt;To start the board recovery, it is recommended to prepare bootable SD card.&lt;BR /&gt;&lt;BR /&gt;Composite firmware image "firmware_ls1046ardb_uboot_sdboot.img" can be downloaded from:&lt;BR /&gt;&lt;A href="https://lsdk.github.io/components.html" target="_blank"&gt;https://lsdk.github.io/components.html&lt;/A&gt;&lt;BR /&gt;section LSDK IMAGES&lt;BR /&gt;&lt;BR /&gt;Using a Linux machine write the firmware image to SD card at offset block (512-byte) 8:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; # dd if=firmware_ls1046ardb_uboot_sdboot.img of=/dev/sdX seek=8 bs=512&lt;/P&gt;&lt;P&gt;(sdX should correspond to actual name of the SD card device)&lt;BR /&gt;&lt;BR /&gt;After preparing the SD card refer to the QorIQ LS1046A Reference Design Board Getting Started Guide, 8 DIP switches (SW5[1:8] + SW4[1]) and set RCW_SRC[0:8] = 0010_0000_0: SDHC/eMMC&lt;BR /&gt;&lt;BR /&gt;Insert SD card and power-on the board.&lt;/P&gt;</description>
      <pubDate>Sat, 07 Aug 2021 09:08:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/No-messages-from-UART/m-p/1319928#M8672</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-08-07T09:08:32Z</dc:date>
    </item>
  </channel>
</rss>