<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: SDK for LS1043A V0.5 environment reset</title>
    <link>https://community.nxp.com/t5/Layerscape/SDK-for-LS1043A-V0-5-environment-reset/m-p/483265#M863</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rommel Custodio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, correct kernel_start should be consistent with flash memory map address as in the doc.&lt;/P&gt;&lt;P&gt;There will be patch for this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Lunmin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Jan 2016 09:34:22 GMT</pubDate>
    <dc:creator>lunminliang</dc:creator>
    <dc:date>2016-01-20T09:34:22Z</dc:date>
    <item>
      <title>SDK for LS1043A V0.5 environment reset</title>
      <link>https://community.nxp.com/t5/Layerscape/SDK-for-LS1043A-V0-5-environment-reset/m-p/483264#M862</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have downloaded the latest QorIQ SDK for LS1043ARDB. I am changing the FW loaded on bank 0 of the NOR flash to SDK v0.5.&lt;/P&gt;&lt;P&gt;Bank 1 is already programmed with a local test FW based on SDK v0.4. Currently, I do not want to change that since it will be my fallback.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems there are discrepancy in the documentation and the actual u-boot code.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Freescale Linux LS1043A SDK, Rev. A, Dec 2015&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #e23d39;"&gt;0x61100000&lt;/SPAN&gt; 0x638FFFFF bank0 FIT Image 40M&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;u-boot&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I have performed environment reset "env default -f -a"&lt;/P&gt;&lt;P&gt;Which cause the LS1043ARDB to cease booting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These environment variables seem to be causing the problem after the environment reset.&lt;/P&gt;&lt;P&gt;kernel_load=0x807f0000&lt;/P&gt;&lt;P&gt;kernel_size=0x1000000&lt;/P&gt;&lt;P&gt;kernel_start=&lt;SPAN style="color: #e23d39;"&gt;0x61200000&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These were reset to SDK v0.4 values and the LS1043ARDB boots now.&lt;/P&gt;&lt;P&gt;=&amp;gt; setenv kernel_load 0xa0000000&lt;/P&gt;&lt;P&gt;=&amp;gt; setenv kernel_size 0x2800000&lt;/P&gt;&lt;P&gt;=&amp;gt; setenv kernel_start 0x61100000&lt;/P&gt;&lt;P&gt;=&amp;gt; save&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #eb7a3d;"&gt;Can someone at FSL verify that these are OK?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jan 2016 05:25:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/SDK-for-LS1043A-V0-5-environment-reset/m-p/483264#M862</guid>
      <dc:creator>rommelcustodio</dc:creator>
      <dc:date>2016-01-12T05:25:20Z</dc:date>
    </item>
    <item>
      <title>Re: SDK for LS1043A V0.5 environment reset</title>
      <link>https://community.nxp.com/t5/Layerscape/SDK-for-LS1043A-V0-5-environment-reset/m-p/483265#M863</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rommel Custodio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, correct kernel_start should be consistent with flash memory map address as in the doc.&lt;/P&gt;&lt;P&gt;There will be patch for this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Lunmin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jan 2016 09:34:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/SDK-for-LS1043A-V0-5-environment-reset/m-p/483265#M863</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2016-01-20T09:34:22Z</dc:date>
    </item>
    <item>
      <title>Re: SDK for LS1043A V0.5 environment reset</title>
      <link>https://community.nxp.com/t5/Layerscape/SDK-for-LS1043A-V0-5-environment-reset/m-p/483266#M864</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;How to install QorIQ LS1043A SDK on Linux machine, please send me the procedure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Raghavendra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jan 2017 10:55:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/SDK-for-LS1043A-V0-5-environment-reset/m-p/483266#M864</guid>
      <dc:creator>raghavendrasurp</dc:creator>
      <dc:date>2017-01-06T10:55:10Z</dc:date>
    </item>
  </channel>
</rss>