<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1046 RESET_REQ_B problem</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046-RESET-REQ-B-problem/m-p/1315544#M8598</link>
    <description>&lt;P&gt;I meet the same problem.I'm very puzzled now.&lt;/P&gt;&lt;P&gt;If I used the RESET_REQ_B of LS1046A to trig a power on reset. LS1046A can not bring up.&lt;/P&gt;</description>
    <pubDate>Fri, 30 Jul 2021 02:15:00 GMT</pubDate>
    <dc:creator>flashingsky</dc:creator>
    <dc:date>2021-07-30T02:15:00Z</dc:date>
    <item>
      <title>LS1046 RESET_REQ_B problem</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-RESET-REQ-B-problem/m-p/904300#M4259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Everybody,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have faced a weird phenomenon on our custom board based on an LS1046A.&lt;/P&gt;&lt;P&gt;In a CPLD I've implemented a power and reset sequence. I was able to bring up our board, the Linux runs correctly from the onboard eMMC, &lt;BR /&gt;BUT,&lt;/P&gt;&lt;P&gt;the LS1046's RESET_REQ_B constantly pulled down. During the reset sequence it goes high then goeas back low&lt;BR /&gt;Despite of this everything seems to be OK.&lt;/P&gt;&lt;P&gt;But I don't understand this phenomenon.&lt;/P&gt;&lt;P&gt;Has anybody faced this before?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance,&lt;/P&gt;&lt;P&gt;Gabor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 May 2019 10:37:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-RESET-REQ-B-problem/m-p/904300#M4259</guid>
      <dc:creator>gaborkocsis</dc:creator>
      <dc:date>2019-05-22T10:37:50Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046 RESET_REQ_B problem</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-RESET-REQ-B-problem/m-p/904301#M4260</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Described behaviour means that there is an issue with RCW.&lt;/P&gt;&lt;P&gt;The first point to check is SerDes reference clocks - they should have correct frequencies and should be provided for all PLLs which are not explicitly powered down in the RCW.&lt;/P&gt;&lt;P&gt;In case of further question please provide the processor connection schematics as searchable PDF for inspection along with U-Boot log.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 May 2019 11:34:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-RESET-REQ-B-problem/m-p/904301#M4260</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2019-05-22T11:34:08Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046 RESET_REQ_B problem</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-RESET-REQ-B-problem/m-p/1315544#M8598</link>
      <description>&lt;P&gt;I meet the same problem.I'm very puzzled now.&lt;/P&gt;&lt;P&gt;If I used the RESET_REQ_B of LS1046A to trig a power on reset. LS1046A can not bring up.&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jul 2021 02:15:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-RESET-REQ-B-problem/m-p/1315544#M8598</guid>
      <dc:creator>flashingsky</dc:creator>
      <dc:date>2021-07-30T02:15:00Z</dc:date>
    </item>
  </channel>
</rss>